STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Question on SPI communication

Hi I am learning to write driver code for SPI. I have an nucleo-L476RG development board with me implementing full-duplex transmit only operation and reading the output of a MOSI pin using a logic-analyzer. The Nucleo board is working as the masterSo...

0693W00000JPooRQAT.png 0693W00000JPoobQAD.png
Tbone1 by Associate II
  • 4303 Views
  • 8 replies
  • 0 kudos

how to transmit an array with HAL_SPI_Transmit_DMA?

Could you please explain me how to use HAL_SPI_Transmit_DMA with an array?In this caseuint16_t data1= 1024;HAL_SPI_Transmit_DMA(&hspi1, &data1, 1)I get a warning concerning the pointer ("passing argument 2 of 'HAL_SPI_Transmit_DMA' from incompatible ...

Tommino by Senior
  • 12742 Views
  • 10 replies
  • 0 kudos

No stuffing bit with HAL_CAN on STM32f4

Hello, I m using the CAN bus on a STM32f412. It is connected to a transiver with a CAN analyser linked. I can receive messages without problem but i can t send any messages. Here is ho i configured the CAN :/*##-1- Configure the CAN peripheral ######...

0693W00000JQ3lXQAT.png
AGiry.2 by Associate II
  • 1644 Views
  • 2 replies
  • 0 kudos

About NUCLEO-F446RE current consumption

Dear Sir・I want to use NUCLEO-F446RE as a PoC for IoT.・I plan to use alkaline batteries and connect to CH6 PIN4. (3.3V)⇒It is necessary to reduce the current consumption.I investigated with a simple FW.(Use stabilized power source(SPS))Case:Run Mode(...

KHosh.1 by Associate II
  • 987 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.