STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems changing settings for different ADC sources

HiI’m having some problems using the ADC on external and internal signals with different requirements.It and old design having a new MCU (STM32L452RCT), where only the MCU interface are updated, the application are (almost) unchanged. The PCB are in ...

JohnnyK by Associate II
  • 2873 Views
  • 6 replies
  • 0 kudos

Resolved! How can ı use the FPU (Floating Point Unit) in STM32F407?

Hİ. I have been working on motor control applications. There are PID, FOC and SVPWM blocks that have contain functions like sin(), cos(), clarke(), park() etc. I used CMSIS DSP library called "arm_mat.h". My microprocessor is STM32F407 M4. I can cont...

"Port Open and try to configure the board"

Hello!I am having trouble when connecting STM32 to Motor Pilot. I am using F302R8 control board and IHM07M1 as power board. I can see the port in Decive Manager and it says it is port COM5, but when I connect through COM5 from Motor Pilot I get the m...

EBerg.2 by Associate II
  • 4537 Views
  • 5 replies
  • 0 kudos

Incorrect interrupt time

Hi everyone,I'm using Nucleo H723 board. I have used 8 timers in encoder mode to read the encoders. I have also activated another timer to make an interrupt every 4ms to send the data via Usart.everything work good but when I use sprint code to put t...

0693W00000KaQ7ZQAV.png
Nmo.1 by Associate III
  • 3791 Views
  • 7 replies
  • 0 kudos

Ambiguous data over MISO Line SPI Communication (Master mode).

Hi all,I am using STM32F334 for SPI communication with a TDC7201 chip from TI.I am using the Low-Level Drivers to initialize the driver and communicate. Here is my initialisation routine: __HAL_RCC_SPI1_CLK_ENABLE();   LL_SPI_InitTypeDef SPI1I...

0693W00000KaEQFQA3.png 0693W00000KaET9QAN.png
AT.8 by Associate II
  • 5329 Views
  • 15 replies
  • 0 kudos

Resolved! Sending USART message via interrupt using registers

Hello,I am working on a college project and struggle with sending a message to the virtual terminal using USART interrupt.I work with following code:void UART_Send (uint8_t *buffer){ USART1->CR1 |= USART_CR1_TXEIE; // Enable TXE Interrupt USART1-...

UMilo.1 by Associate III
  • 3419 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.