2021-06-10 2:25 AM
Hello!
I am having trouble when connecting STM32 to Motor Pilot. I am using F302R8 control board and IHM07M1 as power board. I can see the port in Decive Manager and it says it is port COM5, but when I connect through COM5 from Motor Pilot I get the message "Port Open and try to configure the board" and I am unable to do anything at all in Motor Pilot. I have no clue what this means.
Regards,
Emelie
2021-06-10 7:23 AM
I have configurated the board as the manual says, the message is still there. USART2 is set in the "Connectivity"-category and MotorControl is set in the "Middelware"-category (maybe this is the problem?).
2021-07-30 6:16 AM
I'm facing the same problem on EVSPIN32F02Q1S1.
The Motor Pilot Software says Port Open and try to configure the board when I click on connect.
@EBerg.2 I don't think there's a problem with the MX Configuration. I think something is occupying the COM Port.
I'm stuck, not able to find answers anywhere.
2021-07-30 6:20 AM
Hi @EBerg.2
Didn't take long.
I was using the wrong baud rate aka "Speed" adj to Connect button.
The error isn't user friendly.
The correct speed fixed it
Regards,
Vineeth
2021-10-17 11:18 AM
Hi in my case i changed the boudrate to115200 and now it works well. LG Thomas
2022-02-25 3:32 AM
Check the no. of shunts for which you have configured the IHM07M1 w.r.t code generation, & update the STLink through UTILITY.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.