STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Questions about ST's BFB workaround on STM32L072

I'm working on a STM32L072, and I want to implement an update over the air. I saw there is an errata about the dual bank boot, and ST has made a workaround on it, and it uses the EEPROM.Code from the errata sheet:void SystemInit(void) { /* ...

Ppeyr.1 by Associate III
  • 769 Views
  • 0 replies
  • 0 kudos

FATFS -SDMMC - DMA transfer problem

In CubeMX 5.3.0 I have configured FATFS and FREERTOS for a card running STM32L431. The HAL SDMMC driver is communicating with SD card, and everything goes well until the FATFS want to read the MBR block from the SD card. In this case, the DMA channel...

0690X00000ArmcOQAR.png 0690X00000ArmbuQAB.png
mads.l by Associate II
  • 1359 Views
  • 1 replies
  • 1 kudos

STM32U575 ADC sampling issue

HelloI use a STM32U575 develop board to do the ADC sampling. The inject signal is 10mV RMS with 1.648V bias voltageHowever, from the sampling result, there is a obviously break point in the result.Could you help explain the reason and how to eliminat...

YFANG.2 by Associate III
  • 3193 Views
  • 2 replies
  • 0 kudos

DMA buffer Question

I am trying to send large streams of data into the STM32H753 and I'm trying to maximize the baud rate, ideally aiming for a baud rate of 921600. Unfortunately, I don't know the byte size that will be incoming, which makes it difficult to know how to...

JayDev by Senior II
  • 3581 Views
  • 5 replies
  • 0 kudos

Resolved! How to made a function to call other functions?

Hi to all!!!I do repeteadly this function:switch(segundero_d){case 0: numero_0(); break;case 1: numero_1(); break;case 2: numero_2(); break;case 3: numero_3(); break;case 4: numero_4(); break;case 5: numero_5(); break;case 6: numero_6(); break;case 7...

Systick only runs when CPU is active

I've got a strange situation. I've enabled systick, but it doesn't keep time unless the CPU is active. Key excerpts:main.c: SysTickInit(sys_clocks.SYSCLK_Frequency);void SysTickInit(unsigned base_freq) { SysTick->CTRL = 0; // Turn it off. ...

RSext by Associate II
  • 8983 Views
  • 12 replies
  • 9 kudos

STM32H7 HAL_Delay(200); Problem

This is my first time working with STM32H7B3IIT6 MCU. I wanted to make a led blink application, but the program is HAL_Delay(); it goes into an infinite loop and doesn't exit.

0693W00000JOa2qQAD.png 0693W00000JOa27QAD.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.