STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32h743 adc1 eos flag will not be set until I read the DR

Hi all, recently I am trying to use ADC to sample 4 channel current signals. Since there is no critical time requirement, I plan to use scan mode. In my opinion, the ADC will automatically complete four channel signal conversion stuff, then set the...

Whono.1 by Associate II
  • 5405 Views
  • 7 replies
  • 5 kudos

STM32L4Rxxx OctoSPI with PSRAM

Dear All,In "RM0432 Reference manual STM32L4+ Series advanced Arm ® -based 32-bit MCUs" in chapter "19.3 OCTOSPI implementation" and table "Table 119. OCTOSPI implementation" there are some differences in supported features between families. All fami...

Resolved! INVPC occurs when SVC Handler returns

I use STM32F1 Value Line Discovery Kit.​I want to write SVC handler.If I implement the following, invpc occurs when running 「POP PC�?in Line 38.Caller -------------------------------- __asm volatile(" SVC %0 \n" : : "I" (2)); ...

Myasu.1 by Senior
  • 2126 Views
  • 4 replies
  • 0 kudos

STM32F103C8T6 sending data over I2C via DMA

Greetings!I have "blue pil" stm32f103c8t6 and I want to send data over I2C via DMA. "Classic" way is working fine (I'm sending data to 2004 display through PCF8574 extender), but I can't get it working with DMA.BTF flag isn't set and the loop becomes...

STM32G474 CAN FD no priorization of CAN IDs?

I have multiple CAN FD Participant which are configured the same way:if (canFdMode == canFdModes_2mbit) { hfdcan1.Instance = FDCAN1; hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1; hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_BRS; hfdcan1.Init.Mod...

ATrug.1 by Associate II
  • 1127 Views
  • 1 replies
  • 0 kudos

is it possible to use another output than MCO to generate an arbitrary clock (16.777216MHz) from an internal PLL block?

I want to use a different PLL block than PLL1 to leave PLL1 specific to SYSCLK generation; and for example use PLL2 to generate my arbitrary clock.I see that SAI blocks use for example PLL2 or PLL3 but I don't know if it is possible to make an arbitr...

Pintoo by Associate II
  • 4871 Views
  • 13 replies
  • 0 kudos

32F417 ADC conversion time - figures don't make sense

Hi All,I am using the simplest mode, single conv, software start, etc. 21MHz clock (/2 divisor).I have been measuring the conversion times both in a loop and with a scope on a waggled GPIO pin.With a sampling interval of 3,56,480 I see conversion tim...

PHolt.1 by Senior III
  • 1165 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.