STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to define UART RX pin in initialization? Should we define as alternative function push-pull or floating pin? And why?

We are using STM32F103VCT6 in our projects. We are communicating through RS-485. When we initialize RX pin as alternative function push-pull there occurs a voltage drop on RX pin voltage level. We are curious about UART peripheral GPIO diagram. And w...

NArsl.1 by Associate
  • 1943 Views
  • 1 replies
  • 0 kudos

External Flash Loader don't work

Hello, I am developing an external flash loader using Spi (W25Q16DV) with Stm32G070.Yes, the operation is going well without any problems.However, the peculiar thing is that it doesn't work when you write the user program in the internal flash and ru...

lhwa .1 by Associate II
  • 6093 Views
  • 4 replies
  • 0 kudos

Resolved! I am struggling trying to locate a library header in a specific address. Header has a limited size Error is: ld.exe: DiscoL496_07.elf section `CLIENT_HDR' will not fit in region `CLIENT_ROM' ld.exe: region `CLIENT_ROM' overflowed by 269730352 bytes

The structure of the code is:A library called "clientManiobra.a" to be placed in "CLIENT_ROM" memory region. Library requires to place a struct constant in the very first position in "CLIENT_ROM" memoryThe above library to be linked with main applica...

DBara.3 by Associate II
  • 3709 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F030 High current in stop mode

I would like to put STM32F030K6T6 into STOP mode (low power mode), in which there should be current consumption around 5 μA.But whatever I do the current consumption is around 450 μA in stop mode.There is basically nothing else on the PCB, it's as si...

STM32G474: CAN-Bus clock and timing setup

Hello,regarding the STM32G474 I have some questions regarding the CAN Controller:1)    The CAN-Controller has an input called “fdcan_clk�?, is this connected to APB1-peripheral-clocks?2)    How does the CCU work to generate the fdcan_tq_ck, how shoul...

0693W00000GXU7bQAH.png 0693W00000GXU7WQAX.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.