STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F469-disco CAN-display (I2C) problem

I declare that I am using a CAN library which works with other boards, so right now I’d like to rule out that’s the problem.Therefore, despite having configured the CAN and the code compile correctly, the messages are not received while using STM32F4...

Klaus3 by Associate II
  • 928 Views
  • 0 replies
  • 0 kudos

STM32H750 QUADSPI FIFO Question

I read in the reference manual that the STM32H750 has a 32-byte fifo. FTHRES is the FIFO buffer and FLEVEL indicates how many values ​​are stored in the FIFO buffer. The reference manual also explains that after the FIFO is full the QSPI peripheral t...

0693W00000NpMixQAF.png
JCuna.1 by Senior
  • 985 Views
  • 0 replies
  • 0 kudos

Почему �? не могу загрузить программное обе�?печение дл�? программировани�? STM32F4XX

Загрузка �? �?айта не возможна дл�? �?качивани�?, Как работать �? STM32F4XX контроллерами нет возможно�?ти запрограммировать. �?ужна программа ST SW-STM32065 и Keil μVision, а �?качивать не разрешает.

STM32F407 USART6 DMA not receiving data

I have configured 2 UARTS both are configured to using HAL_UARTEx_ReceiveToIdle_DMA.My init functions:HAL_UARTEx_ReceiveToIdle_DMA(&huart3,aRxBuffer, RXBUFFERSIZE);   __HAL_DMA_DISABLE_IT(&hdma_usart3_rx,DMA_IT_HT);       HAL_UARTEx_ReceiveToId...

0693W00000NpHt7QAF.png
LPetr.1 by Senior II
  • 6394 Views
  • 13 replies
  • 0 kudos

Power supply without regulator

Hello,I am currently working on my end of year project. I first realized my project under a development kit then now I realize the PCB.I am currently facing a problem. I have an STM32L073RZ which I must supply. As a power supply, I have a Li-SOCl2 ac...

I have a STM32H7 project and want to use the DMA for peripheral data transfer with an external static DMAREADY input

When using an EXTI input to trigger a DMA request, there is only the possibility to trigger on falling or rising edged of the input. But my peripheral has only an output which is active when data are ready for read or write. This output is static and...

JKuen.2 by Associate II
  • 2824 Views
  • 4 replies
  • 0 kudos

FDCAN Tranceiver on STM32G0B

Hi all,I have a CAN 2.0 network up and running with a F407 and some F103. I added a board with a G0B (fdcan). I couldn't get my hands on a FDCAN-tranceiver. I tried to get it working in classic mode (from repository example) with a CAN2.0 tranceiver....

PDeng.1 by Associate
  • 747 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.