STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is connected to the ''internal wakeup line''

Posted on February 02, 2017 at 10:59Hello,reference manuals for the L4 series in the power section talk about a EIWUL bit in the PWR->CR3 register, enabling an 'internal wakeup line'. A search in the manuals and with google does not bring up any fur...

Resolved! Problems saving variables to FLASH in STM32G030F6P6

I've just bought a STM32G030F6P6 dev board and I'm testing its cababilities.And one thing I'm having problems with is saving my data to the FLASH.The first time it writes as espected in the FLASH, but not in the second, HAL_FLASH_Program returns HAL_...

arthhh by Associate II
  • 1690 Views
  • 2 replies
  • 0 kudos

STM32H743 Can BDMA trigger a DMA2 transfer

I already set up a SPI1 Tx and Rx with MDMA and DMA2 moving data from DTCMRAM to RAMD2 to SPI1Is it possible to do the same with SPI6 ?I see that DMA2 can access APB4 peripherals (including SPI6) but "sp6_rx_dma" and "spi6_tx_dma" hardware requests a...

Resolved! I want to send 16-bit numeric 16-channel data measured by ADC with BLE. However, when programming according to the BLE example, the transmitted data is in the form of 8 bits. What is the general way to solve this?

I want to send 16-bit, 16-channel data measured by ADC. but I realize BLE is transfering 8bit data. How can I solve this?my key script is below.<main.c>uint16_t DMAo[16];​ HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED); HAL_ADC_Start_DMA(&hadc...

KKIM.6 by Senior II
  • 2040 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.