STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART and timer interrupt issue

Hello! Can you help me?I'm receiving data in UART Rx with DMA and send it by USB, it works fine. Now i'm trying to set up a timer to check if I'm receiving data every 250[ms] and send a special message. When I don't configure the timer it works, but ...

SGonz.2 by Associate II
  • 5849 Views
  • 2 replies
  • 0 kudos

STM32F030 Temperatur Sensor

i tried to use the internal temperatur sensor but its a little bit strangewhen the tempertur goes up the value from the adc goes downis that right or is my config for the adc wrong ?

RSeye.1 by Associate II
  • 3292 Views
  • 7 replies
  • 0 kudos

Setting Option Bytes on a new MCU fails on STM32L451RCT6

Hello eveyone,In my code i try to set the BOR level with the following function:/** * Set proper BOR level. */ void setBorLevel(void) { FLASH_OBProgramInitTypeDef optionBytesInit = {0U}; bool_t isBorLevelConfigured; uint32_t borLevel = ...

AH.6 by Associate
  • 1051 Views
  • 0 replies
  • 0 kudos

stm32L051 registers don't change

Hello!I'm working on a custom board with an stm32L051 and the HSI16 crystal. I'm setting the clock registers, Flash, PWR and then I try to enable the clock for TIM21. as you can see in the code I set the bit but the computer "doesn't listen"(I am loo...

0693W00000NrKBMQA3.png
EPora.1 by Associate II
  • 2259 Views
  • 6 replies
  • 0 kudos

Resolved! About output compare mode of STM32G071RB

I want to perform a timer interrupt using the output comparison mode.When the frequency is set to 2000Hz, ARR : 20, CCR1 : 25, I think that interrupt does not occur because ARR <CCR1, but interrupt occurs. Why do interrupts occur?

0693W00000NrN36QAF.png
Sodag.1 by Associate II
  • 1742 Views
  • 3 replies
  • 0 kudos

the touchscreen on the board STM32H747I-DISCO

Hello,I need some examples to learn how to configure and use the touchscreen on STM32H747I-DISCO board.Could you provide it or direct me to the resources which contain such an example, please.Thanks,Best regards

DShub.1 by Associate II
  • 847 Views
  • 0 replies
  • 0 kudos

STM32H7 HAL QSPI delayed clocks

I'm reading data from an FPGA over QSPI. I'm attempting to read 256 bytes at a time. However, when I read the data the QSPI clock decides to take a long pause before continuing. I get an initial burst of 74 clock pulses, then 56 bursts of 8 clock pul...

0693W00000NrMdrQAF.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.