STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 MCU with J-link programmer

I'm using Segger's J-Link programmer to program STM32F767 MCU. Quick Question:1) During programming/flashing (while downloading a binary file), J-Link programmer asserts RESET# line logic LOW or RESET# line will logic High?

S.Kamath by Associate III
  • 1704 Views
  • 1 replies
  • 0 kudos

How do I get Timer8 Compare to toggle an output pin?

Working with TIM8; I have enabled one-time-pulse, set 'Channel1' to 'Output Compare CH1', set the Output Compare Channel 1 Mode to 'Active Level On Match', and Pulse to 0. I set the timer's ARR = 65535, and set the Compare Register to 20000. I hav...

LMorr.3 by Senior II
  • 1785 Views
  • 2 replies
  • 0 kudos

Using JTAG and SPI1_MISO on PB4

As soon as i configure PB4 as SPI1_MISO, I get disconnected from the target. Even the connection doesn't use the NJTRST pin.It used to be a bug on the stm32L4, but I could't find it mention on the errata of the stm32U585.Has anyone (ST) knowledge abo...

aritec by Associate III
  • 3731 Views
  • 7 replies
  • 0 kudos

X-CUBE-WIFI1 with STM32F070

Hello,I am trying to develop an application with the X-NUCLEO-IDW04A1 Wi-Fi evaluation board on a STM32F070 microcontroller. I downloaded the expansion package X-CUBE-WIFI1 that provides implementations for STM32L0, L4, F1 and F4 but not on my target...

TRand.1 by Associate
  • 2267 Views
  • 2 replies
  • 0 kudos

Weird Memory Fault Error In STM32H7.

Hello,I am working on a empedded firmware development which uses RTOS RTX5, running on STM32H753ZI microcontroller. I have set up a web server and I receive and send JSON. The library I am using to create and Parse JSON is CJSON. Everything work well...

SEfte.1 by Associate II
  • 828 Views
  • 0 replies
  • 0 kudos

How should I configure SDMMC1 for STM32H747I-DISCO?

I try a lot of clock configurations but it always response command timeout error at the following line of the generated MX_SDMMC1_SD_Init function.if (HAL_SD_Init(&hsd1) != HAL_OK) {  Error_Handler(); }How should I set the SDMMC1 configuration for ST...

Ellaine by Associate II
  • 2275 Views
  • 3 replies
  • 0 kudos

UART and timer interrupt issue

Hello! I having some problems using USART and timersI'm receiving data by USART1+DMA and sending it by USB every 100[ms], if no data is received in 1[s], then timer TIM2 make an interrupt and sends a special USB message. This is done resetting timer'...

SGonz.2 by Associate II
  • 1463 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.