STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello! I purchased the STM32G431RBT-Nucleo board. When trying to write code to control the DAC, I ran into a problem - regardless of the code change, the result is 0v, there is a straight line on the oscilloscope. The code itself runs on STM32F407. Do you

One of the variint main(void){ /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /...

DTorn.1 by Associate II
  • 4428 Views
  • 17 replies
  • 0 kudos

Is system memory protected from read?

Recently we have received STM32F103RBT6/T7 samples which could not be flashed using internal bootloader. We have checked working devices and under 0x1FFF F000 they have readable bootloader firmware code. Problematic samples have FF bytes in the same ...

ROlej.1 by Associate
  • 1220 Views
  • 1 replies
  • 0 kudos

STM32F777 Parallel Bus Interface

Hi,I am working on STM32F777 MCU LQFP 176 Package.I need to confirm if i can use FMC interface with my EtherCAT chip FIDO5200 that uses 16-bit data lines and 4-address lines.Also I need to interface SRAM (parallel bus)that has 8-bit data and address...

RSHAR.2 by Associate II
  • 4089 Views
  • 5 replies
  • 0 kudos

Capture input PWM analog signal using Timers.

I have a specific requirement to capture input PWM analog signal using Timers.The timer should capture both period and duty cycle of the input signal for one pulse, then stop the capture automatically.The application can read the capture compare regi...

Shakthi by Associate II
  • 1180 Views
  • 1 replies
  • 0 kudos

Backup SRAM duration

Hi STM,I am having short question about BACKUP SRAM on STM32F437 MCU. So, for how long will BACKUP SRAM keep data, if power supply is removed. Will the data stay there, after some long period or will they be wiped out?If they are going to be wiped ou...

AKara.9 by Associate II
  • 2721 Views
  • 5 replies
  • 0 kudos

CAN1_RX0 interrupt not firing

I've been working on getting the STM32f7-EVAL operational to later on migrate it to STM32F767II. For this we decided to split up functionality into 3 sections, there is a forward facing application that has the main and specific business logic.Curren...

JChri.7 by Associate
  • 920 Views
  • 0 replies
  • 0 kudos

Alternate Function 0 in STM32

In my STM32, if I have set the GPIO_MODER as "Alternate function" and did not set any values in the GPIO_AFRL and GPIO_AFHL, I guess it will take the defaukt value of AF0. What is AF0 used for ?

SNara.6 by Associate II
  • 3042 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.