STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 QSPI FLASH write issue

Hello,I am working with STM32H743BI and trying to write then read a QSPI FLASH "mt25qu01gbbb". I first use the STM32 software example "QSPI_ReadWrite_IT" (adapted with cube configuration) to start discovering QSPI on my hardware. Then I made a small ...

0693W00000QLm9HQAT.png 0693W00000QLm3sQAD.png

Force BLE disconnection from peripheral device

Hello everyone, Can I in any way force disconnection from peripheral device?I’m using BlueNRG-LP MCU and BLE Stack APIs. I want to force a disconnection with the central from my peripherals. Is it possible with BLE?I would like to avoid a reset softw...

ARamí.1 by Associate II
  • 937 Views
  • 0 replies
  • 0 kudos

QSPI reading and Writing function not showing correct data

hi, I am trying to implement QSPI in STM32H743 with S25FL512. REad ID function work properly, showing correct data like command 0x9Fresult: {01}{02}{20}{4D}{00}{80} memory size 65Mbytebut the BSP_QSPI_READ/WRITE function not correct data, some one gu...

ykn by Senior
  • 1275 Views
  • 1 replies
  • 0 kudos

STM32H745 Disco, Simple Hello World and LED Blink

I have worked with several STM32 Nucleo and Discovery Boards. My typical starting point is to print "Hello World" and blink an LED with from a HAL project. The HAL/IOC part is working as expected. I am thinking I am missing some dual-core hardware ...

DDilw.1 by Associate
  • 3167 Views
  • 1 replies
  • 0 kudos

How can I connect Gbit SDRAM to STM32F429?

Hello, I would like to connect Gbit SDRAM to STM32F429 MCU. When I look at the STM32 FMC memory map, it has two 256 Mbytes area for SDRAM. As far as I understand, I can connect up to 4 Gbit SDRAM. However, SDRAMs have maximum 512 Mbit size. 1) Is it ...

I am using STM32F417IEH6 on a custom-board with Azure_RTOS. The Azure_RTOS/ThreadX is working OK. I have several threads running.

 My board is supposed to act like a PM-bus server on top of a ATX-PSU and I need to 'time' the sequence, that powers up the PSU. I have tried to use 'tx_thread_sleep()' and even changed tx_user.h : #define TX_TIMER_TICKS_PER_SECOND        --> 1000 an...

olebenny by Associate II
  • 736 Views
  • 0 replies
  • 0 kudos

When to stop TIM_DMABurst and how to first start TIM_DMABurst

I try to use TIM_DMABurst to generate exact number of pwm pulses.But I found after call HAL_TIM_DMABurst_WriteStart and HAL_TIM_PWM_Start, it enter HAL_TIM_PeriodElapsedCallback. And then if I call HAL_TIM_PWM_Stop it will stop and generate no pwm. I...

dming.4 by Associate II
  • 3907 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L4 : IWDG wake up device in shutdown mode ?

Hi !I'm using the stm32l452RE mcu and I use the shutdown mode. I also use the watchdog (IWDG) to reset the system if an error occurs. This IWDG is set to 4s. When I go in shutdown mode, accordly to the docs, IWDG should be off because it is clocked w...

SimonF by Senior
  • 12172 Views
  • 20 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.