2022-07-22 3:19 AM
My board is supposed to act like a PM-bus server on top of a ATX-PSU and I need to 'time' the sequence, that powers up the PSU. I have tried to use 'tx_thread_sleep()' and even changed tx_user.h : #define TX_TIMER_TICKS_PER_SECOND --> 1000 and tx_initialize_low_level.s : SYSTICK_CYCLES --> SYSTICK_CYCLES = ((SYSTEM_CLOCK / 1000) -1 to achieve 1 mS. But this is still not accurate enough.
How can I get better control ??
I need to : turn ON 12V --> wait some time --> turn ON 5V --> wait some time --> turn ON 3V3.
Are there any free running counters, that I can read/poll ??
Or ??
Olebenny
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.