2022-08-16 11:43 AM
Hi I am using STM32G030F6 I am try to programing UART 1&2. UART2 is working fine with transmit & receive data. But UART1 only able to transmit data not able received.
Please let me is there any settings is required.
2022-08-18 7:47 AM
Hi @dsapk.1 and welcome to the Community :),
Try to use only USART1 and check if you can receive data.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.