Ask questions, find answers, and share insights on STM32 products and their technical features.
stm32cube mx just generate flash.ld linker script. So I create my own ram.ld linker script, also i modify system_stm32g0xx.c to point the entry point to sram /* Note: Following vector table addresses must be defined in line with linker confi...
Hi,In the snippet below, comment says select PLL as system clock but in code it is configured as HSE clock which one shall be considered? /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 clocks dividers */ RCC_ClkIni...
For the package LQFP48 the pinout is the same. Also Pin names are the same. So is it possible ?
Hi,I'm testing running a relocatable binary model.But when I use ai_rel_network_run(), I get into HardFault.The detailed error information is as follows, with my current test code attached.Hope that someone can help to resolve this issue!Thanks. /* U...
I am a bit frustrated with the USART2, which is connected to the UART9 TX9-RX2 and TX2-RX9. So with sending from TX9 to RX2 everything is fine but the other way around there is a first byte = 254d inside the receive buffer. huart2 and huart9 are init...
Hello together,im using in my project the µC "STM32F302C8T6-LQFP48 pinout" on a self designed PCB with another HW-components and a part of this project is to measure ADC values, which I do over DMA. Generally, it is working, (when I supply only the P...
Hi everybody, I'm trying to delete a single sector of my STM32L4P5G Discovery Board MX25UM51245G OctoSPI Flash memory but I always end up in a timeout. Reading memory by function BSP_OSPI_NOR_Read() is working as expected. I'm using the bord support ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.