STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 U575 LSE Clock doesn't start.

LSE clock is set in the Cube and initialisedAfter intitialisation the following registers are not set correctly and the LSE clock isn't calledRCC->BDCR->LSEDRIVE not set to hight event though macro calledRCC->BDCR->LSCOSEL set to LSIRCC->BDCR->LSCOEN...

sneal by Associate II
  • 4184 Views
  • 7 replies
  • 0 kudos

stm32 uart interrupt stops working after ~1 hour

I am using an STM32L073 chip. I have 2 UARTs but only the huart1's receive is using interrupts. I start the Rx interrupt at start-up and then the interrupts are being set at the end of the interrupt function. (see code below)My issue is that after ab...

VWied.1 by Associate III
  • 8257 Views
  • 8 replies
  • 2 kudos

Hi, i have a problem with my Hardware Flow Control on my STM32F103RBT6. I send a UART Signal with Polling but the STM neither sets the Signal on the USART Tx Pin nor does it set the RTS Pin. Please help me to find a solution. Thank you!

The STM does send the Signal if i set the RTS Pin on high level per software:USART2->CR3 |= 0x0100; //RTSE->1The Problem is i use a three state Buffer Line Driver (74HC126D) in order to enable transmitting or receiving but the RTS Pin from the STM is...

SJank.3 by Associate III
  • 5087 Views
  • 5 replies
  • 0 kudos

I need design "CAD" resources for STM32F205

Hello,Recently I moved a design to the STM32L552 because I wanted an extra layer of security and protection for my IP. Also, the device has some new features that I plan to adopt in the new design, like the DMAMUX. On the other hand, it's been a whil...

Zaher by Senior II
  • 1404 Views
  • 2 replies
  • 0 kudos

Resetting CNDTR for UART DMA method

I'd like to set the counter of huart2.hdmarx->Instance->CNDTR;To reset the buffer index.How is this done?nevermind. The peripheral required disabling first it seems.huart2.hdmarx->Instance->CCR &= ~DMA_CCR_EN; // disablehuart2.hdmarx->Instance->CNDTR...

d4 by Associate III
  • 3209 Views
  • 1 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.