STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I want to generate ONE PULSE TRIGGER by comparing the encoder counts input from 2MHz to 4MHz and setting the delay time and duty.

hello.​I want to generate ONE PULSE TRIGGER by comparing the encoder counts input from 2MHz to 4MHz and setting the delay time and duty.​Currently on TIM6void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) is used and trigger is generated usi...

rm.1 by Associate II
  • 2060 Views
  • 4 replies
  • 0 kudos

STM32L011K4T - MCU ADC Temperature

Posted on February 06, 2018 at 01:23 Hi, I would like someone to confirm that the temperature I am getting is somewhat in the ballpark to be expected. If it isn't, could someone check my values that I am using from the datasheet? I am curre...

0690X00000609cnQAA.png
Nolan L by Associate III
  • 3934 Views
  • 4 replies
  • 0 kudos

STM32H7 Unique 96-bit serial number is really Unique ??

We are looking for Unique identification number per STM32, in the process we came to know about unique 96-bit serial number. is it really Unique ?? how it Guarantees, that no duplicate exist ??Can you please help on this clarification ??INFO

0693W00000UFS83QAH.png
SPati.7 by Associate III
  • 2544 Views
  • 4 replies
  • 0 kudos

STM32L486Z6Tx as an SPI slave with DMA

Hey I am using a STM32L486Z6Tx as an SPI slave, the device transfers blocks of 3588 bytes (512*7 + 4 byte checksum). At spi clock rates up to 1.2MHz everything works as planned. However at higher clockrates I still receive all my data, the checksum p...

LM.2 by Associate II
  • 1123 Views
  • 0 replies
  • 0 kudos

Resolved! How ARR value impact on timer input capture result?

Hello guys,I have just started working with stm32 controllers. I am trying to capture the frequency of signal using timer 2 input capture mode.I am getting absolutely correct frequency if i use ARR = 65535 but when i use ARR = 0xffffffff (As timer 2 ...

HB by Associate II
  • 14304 Views
  • 26 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.