2022-09-29 3:16 AM
Hi every one; using a STM32-F401RE board , how can i canghe on the fly the period and duty cycle of the two signal got in complementary PWM death time using ARR and CCR register?
2022-09-29 3:18 AM
Starting the timer in this way:
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);
and using this call back:
void HAL_TIM_PeriodElapsedCallback (TIM_HandleTypeDef *htim)
doesn't work
2022-09-29 6:34 AM
Check if you have enabled the timer interrupt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.