STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Continuous SPI transactions using DMA

A little background first. I'm use the STM32F412 in a custom design and not using STM32Cube packages.What I want to do is continuously transmit/receive a fixed number of bytes on a SPI interface (master) using DMA with no software interaction (i.e. n...

KSGreenA by Associate
  • 1635 Views
  • 1 replies
  • 0 kudos

Resolved! ADC Sequence conversion not working on STM32G030. Only a single EOC and EOS event when CHSELR = 0b111.

I have tried multiple different configurations, software trigger, hardware trigger, the only way to read ADC channels in sequence is to use DISCONT=1 and trigger each reading individually. I have minimized my project to a testcase where a software tr...

deltronix by Associate II
  • 2727 Views
  • 3 replies
  • 0 kudos

STM32H730 SPI clock (SCK) bug

Hello.I have noticed a SCK clock error on the SPI bus in the STM32H730 processor. It may be due to the HAL library I am using (v1.10.0).My SPI configuration (SPI2 in this case) in CubeMX:I use SPI in Polling Mode. I send 8 bits of data using the func...

0693W00000UnwXaQAJ.png 0693W00000UnwXkQAJ.png
Kubeck by Associate II
  • 3457 Views
  • 5 replies
  • 0 kudos

Resolved! Where are the project-files, empty folder?

Hello,I have created a sample project from Stm32CubeIDE, but there are no files in the specified location folder, see attached image.I do not understand this? Where are the files? How is this linked?Thank you

pk84 by Senior
  • 2897 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.