2022-10-12 4:56 AM
Hey I'm trying arm keil to run my code but I'm facing an error.
here is files link https://drive.google.com/open?id=1XFlZseg42zr7erE-cU_o2zDSs3MlGWXf&authuser=ashutamar0%40gmail.com&usp=drive_fs
here is an error
*** Using Compiler 'V6.18', folder: 'C:\Keil_v5\ARM\ARMCLANG\Bin'
../USER/main.c(15): warning: In file included from...
../Libraries/CMSIS/CM3/DeviceSupport/ST/STM32F10x\stm32f10x.h(461): warning: In file included from...
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1204): error: unknown type name 'inline'
static __INLINE void __enable_irq() { __ASM volatile ("cpsie i"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1205): error: unknown type name 'inline'
static __INLINE void __disable_irq() { __ASM volatile ("cpsid i"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1207): error: unknown type name 'inline'
static __INLINE void __enable_fault_irq() { __ASM volatile ("cpsie f"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1208): error: unknown type name 'inline'
static __INLINE void __disable_fault_irq() { __ASM volatile ("cpsid f"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1210): error: unknown type name 'inline'
static __INLINE void __NOP() { __ASM volatile ("nop"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1211): error: unknown type name 'inline'
static __INLINE void __WFI() { __ASM volatile ("wfi"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1212): error: unknown type name 'inline'
static __INLINE void __WFE() { __ASM volatile ("wfe"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1213): error: unknown type name 'inline'
static __INLINE void __SEV() { __ASM volatile ("sev"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1214): error: unknown type name 'inline'
static __INLINE void __ISB() { __ASM volatile ("isb"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1215): error: unknown type name 'inline'
static __INLINE void __DSB() { __ASM volatile ("dsb"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1216): error: unknown type name 'inline'
static __INLINE void __DMB() { __ASM volatile ("dmb"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1217): error: unknown type name 'inline'
static __INLINE void __CLREX() { __ASM volatile ("clrex"); }
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1468): error: unknown type name 'inline'
static __INLINE void NVIC_SetPriorityGrouping(uint32_t PriorityGroup)
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(751): note: expanded from macro '__INLINE'
#define __INLINE inline /*!< inline keyword for GNU Compiler */
^
../Libraries/CMSIS/CM3/CoreSupport\core_cm3.h(1489): error: unknown type name 'inline'
static __INLINE uint32_t NVIC_GetPriorityGrouping(void)
^
2022-10-12 5:56 AM
Doesn't seem to be picking up the V6 compiler.
Under the C/C++ settings pick the V5 compiler.
2022-10-13 5:24 AM
Hey Thanks but I'm getting this error now
Tool: ArmCC [4d365d]
compiling list.c...
Error: C9555E: Failed to check out a license.
The license file could not be found. Check that ARMLMD_LICENSE_FILE is set correctly.
ARMLMD_LICENSE_FILE is not set. You must set this to the path to your license.
Information about this error is available at: http://ds.arm.com/support/lic87/m1
General licensing information is available at: http://ds.arm.com/support/licensing/
If you need further help, provide this complete error report to your supplier or license.support@arm.com.
- ARMLMD_LICENSE_FILE: unset
- LM_LICENSE_FILE: unset
- ARM_TOOL_VARIANT: unset
- ARM_PRODUCT_PATH: unset
- Product location: C:\Program Files (x86)\ARM_Compiler_5.06u7\sw\mappings
- Toolchain location: C:\Program Files (x86)\ARM_Compiler_5.06u7\Bin
- Selected tool variant: product
- Checkout feature: compiler5
- Feature version: 5.0202006
- Flex error code: -1
Product: ARM Compiler 5.06
Component: ARM Compiler 5.06 update 7 (build 960)
Tool: ArmCC [4d365d]
compiling queue.c...
Error: C9555E: Failed to check out a license.
The license file could not be found. Check that ARMLMD_LICENSE_FILE is set correctly.
ARMLMD_LICENSE_FILE is not set. You must set this to the path to your license.
Information about this error is available at: http://ds.arm.com/support/lic87/m1
General licensing information is available at: http://ds.arm.com/support/licensing/
If you need further help, provide this complete error report to your supplier or license.support@arm.com.
- ARMLMD_LICENSE_FILE: unset
- LM_LICENSE_FILE: unset
- ARM_TOOL_VARIANT: unset
- ARM_PRODUCT_PATH: unset
- Product location: C:\Program Files (x86)\ARM_Compiler_5.06u7\sw\mappings
- Toolchain location: C:\Program Files (x86)\ARM_Compiler_5.06u7\Bin
- Selected tool variant: product
- Checkout feature: compiler5
- Feature version: 5.0202006
- Flex error code: -1
Product: ARM Compiler 5.06
Component: ARM Compiler 5.06 update 7 (build 960)
Tool: ArmCC [4d365d]
compiling tasks.c...
Error: C9555E: Failed to check out a license.
The license file could not be found. Check that ARMLMD_LICENSE_FILE is set correctly.
ARMLMD_LICENSE_FILE is not set. You must set this to the path to your license.
Information about this error is available at: http://ds.arm.com/support/lic87/m1
General licensing information is available at: http://ds.arm.com/support/licensing/
If you need further help, provide this complete error report to your supplier or license.support@arm.com.
- ARMLMD_LICENSE_FILE: unset
- LM_LICENSE_FILE: unset
- ARM_TOOL_VARIANT: unset
- ARM_PRODUCT_PATH: unset
- Product location: C:\Program Files (x86)\ARM_Compiler_5.06u7\sw\mappings
- Toolchain location: C:\Program Files (x86)\ARM_Compiler_5.06u7\Bin
- Selected tool variant: product
- Checkout feature: compiler5
- Feature version: 5.0202006
- Flex error code: -1
Product: ARM Compiler 5.06
Component: ARM Compiler 5.06 update 7 (build 960)
Tool: ArmCC [4d365d]
compiling port.c...
Error: C9555E: Failed to check out a license.
The license file could not be found. Check that ARMLMD_LICENSE_FILE is set correctly.
ARMLMD_LICENSE_FILE is not set. You must set this to the path to your license.
Information about this error is available at: http://ds.arm.com/support/lic87/m1
General licensing information is available at: http://ds.arm.com/support/licensing/
If you need further help, provide this complete error report to your supplier or license.support@arm.com.
- ARMLMD_LICENSE_FILE: unset
- LM_LICENSE_FILE: unset
- ARM_TOOL_VARIANT: unset
- ARM_PRODUCT_PATH: unset
- Product location: C:\Program Files (x86)\ARM_Compiler_5.06u7\sw\mappings
- Toolchain location: C:\Program Files (x86)\ARM_Compiler_5.06u7\Bin
- Selected tool variant: product
- Checkout feature: compiler5
- Feature version: 5.0202006
- Flex error code: -1
Product: ARM Compiler 5.06
Component: ARM Compiler 5.06 update 7 (build 960)
Tool: ArmCC [4d365d]
compiling heap_2.c...
Error: C9555E: Failed to check out a license.
The license file could not be found. Check that ARMLMD_LICENSE_FILE is set correctly.
ARMLMD_LICENSE_FILE is not set. You must set this to the path to your license.
Information about this error is available at: http://ds.arm.com/support/lic87/m1
General licensing information is available at: http://ds.arm.com/support/licensing/
If you need further help, provide this complete error report to your supplier or license.support@arm.com.
- ARMLMD_LICENSE_FILE: unset
- LM_LICENSE_FILE: unset
- ARM_TOOL_VARIANT: unset
- ARM_PRODUCT_PATH: unset
- Product location: C:\Program Files (x86)\ARM_Compiler_5.06u7\sw\mappings
- Toolchain location: C:\Program Files (x86)\ARM_Compiler_5.06u7\Bin
- Selected tool variant: product
- Checkout feature: compiler5
- Feature version: 5.0202006
- Flex error code: -1
Product: ARM Compiler 5.06
Component: ARM Compiler 5.06 update 7 (build 960)
Tool: ArmCC [4d365d]
".\Obj\Project.axf" - 35 Error(s), 0 Warning(s).
Target not created.
Build Time Elapsed: 00:00:01
2022-10-13 5:49 AM
So a licensing issue with the Keil tools, and the use of an old version of CMSIS libraries that predated, and doesn't recognize, the version 6 compiler.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.