STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can the STM32L4 transmit and receive USART over DMA?

Hello, I am inquiring about USART communication using DMA. I am following github.com/MaJerle/stm32-usart-uart-dma-rx-tx tutorial using the low level drivers for a STM32L432. I have reception working with no troubles and I believe my interrupts are be...

ABicc.1 by Associate
  • 2679 Views
  • 1 replies
  • 0 kudos

I am trying to read 3 ADC channels via DMA. One weird thing happen: if I use a breakpoint on the line of the readings, I get the correct values from the ADC. If I don't use a breakpoint, the values are always 0 or random. Can you help me ?

I tried using delays, but they don't solve the problem. Data are retrieved using HAL_ADC_Start_DMA(&hadc1, value, DATA_LENGTH) HAL_ADC_Stop_DMA(&hadc1);here below my intialization and function:void MX_ADC1_Init(void){    ADC_ChannelConfTypeDef sConf...

LScar.1 by Associate
  • 1311 Views
  • 1 replies
  • 0 kudos

LSE Gain margin

Hi,I am using a crystal from AN2867 (ECX-.327-CDX-1293). I'm having trouble starting LSE on stm32g474 mcu.When I calculate gain Margin, I reach 1.24. The expression in the application note also tells us to be careful that the oscillator transconducta...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.