STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA Mem to peripheral inconsistent output

I have a timer + dma which outputs a signal for addressable LEDS. The code calls the PWM Start function on a crude timer loop for testing purposes.The first time the DMS starts, its perfect, and the output is correct and as expected. However the seco...

0693W00000SuEDcQAN.png 0693W00000SuEDwQAN.png

Resolved! stm32g431 boot 0 pb8

how disable boot 0 pin8 i used this pin for input make problem to boot from flash how can disable any condition mcu boot from flash not check this pin when reset

How is CAN message RAM initialized/zeroed on STM32H7?

I have the problem that the CAN message RAM which is allocated for the acceptance filters is not zeroed out on startup.The part of the CAN message RAM allocated for acceptance filter seems to just be random data which means that usually no CAN frames...

julianoes by Associate II
  • 1500 Views
  • 0 replies
  • 1 kudos

Trying to do an encoder with an FSM

Hello, right now im trying to do an encoder as a project for my digital electronics class. I've done it in two different ways, by functions and by switch cases, and neither seem to work. I have to make it so every time a switch of states ocurr within...

OMart.6 by Associate
  • 1666 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.