STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F207 access data to beyond flash size

I have STM32F207ZE and made a project that read and write data to flash memory.​STM32F207ZE flash size is 512Kbyte.but I tried writing data to a 0x80E0000 address(flash sector 11), it worked.​Surprisingly, the STM32CubeProgrammer can also has access ...

0693W00000WJaEeQAL.png
rndkd1 by Associate II
  • 3162 Views
  • 4 replies
  • 0 kudos

Allocated memory corrupted in Interruptroutine?

Hello Community,I'm developing a program for a STM32 L051R6T6 with CubeIDE.on bare metal, using HAL driver functions.It reads some cyclic data from two USARTS using DMA.The maincycle does processing of the rxTelegrams, transmits and does some logging...

TheaArt by Associate III
  • 2986 Views
  • 4 replies
  • 0 kudos

STM32U585 temperature sensor

HelloCould you share some detail of STM32U585 temperature sensor information?When do the calibration in plant, how to guarantee the junction temperature of the chip? Do you perform the calibration with bare die or with package?How about the linearity...

YFANG.2 by Associate III
  • 7817 Views
  • 14 replies
  • 0 kudos

[STSPIN32G4]Buck or Gate Dirver EMI?

1. Far-field EMI, as shown in the figure below2. MCU Near-field FFT, as shown in the figure below(EVM also has this situation)3. External power connection, as shown in the figure below4. Use a scope carbon rod and use a ground spring. It is measured ...

0693W00000WJak6QAD.png 0693W00000WJajNQAT.png 0693W00000WJaj3QAD.jpg 0693W00000WJal9QAD.jpg
BChen.11 by Associate
  • 960 Views
  • 1 replies
  • 0 kudos

with Evaluation STM32H7 board, LEDs do not work properly.

In my first stm32 project, I wanted to turn on and off LD1~LD4 on EVAL-STM32H757 board.LD2 and LD4 worked good, but LD1 and LD3 did not work.I set IOC file only RCC and GPIO and Clock Configuration with no error.GPIO Pins : PK3, PK4, PK5, PK6 as GPI...

OhBang by Associate II
  • 2248 Views
  • 5 replies
  • 0 kudos

PC Testing equipment for STM32 boards.

I would like to test STM32F4/L4/H7 based boards with emulated testing software on a PC.I need to test all standard serial communication protocols along with injecting external PPS or interrupt.I need an PCI or USB adaptors or cards, and a software AP...

deckhard by Associate III
  • 1847 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.