STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can STM32 chips use any pin?

Coming from AVR this is not possible, I do see some peripherals can use multiple pins. Working with the STM32H7 specifically here. A colleague of mine said he was under the impression ST chips can use any pin ( or a number of pins ) for say one of th...

ulao by Associate III
  • 2464 Views
  • 6 replies
  • 0 kudos

Resolved! Can't flash STM32F411RE from macOS

Hi,i am using macOS to flash an STM32F411RE.It is recognized, the mass storage shows up, but whenever i try to flash it using ArduinoIDE, it exits with code 3: STM32F411RE not found.Does anyone know how to fix this?Thanks in advance.

JNied.2 by Associate
  • 1095 Views
  • 1 replies
  • 0 kudos

Can Anyone guide me in detail how to Measure AC signal 3V, 50Hz using STM32?? I have to find out the RMS value. Since I am new to this can you guide me how to go about ??

I have understood that I have to use Timer to trigger ADC conversion at a configurable sampling frequency. ADC Clock = 24 MHz. I am planning to use DMA also.Can someone help me with calculations and in detail explanation?

STee.1 by Associate
  • 2153 Views
  • 1 replies
  • 0 kudos

Issue to use PC13 as output on RTC wakeup timer

hello all, I want to write a code to test the possibility to use PC13 as output to activate a regulator when the micro is in Vbat mode.. I'm using a STM32F476.in the manual, in Vbat mode, RTC_OUT still available for Alarm ou wakeup output.so, in cube...

Seth1er by Associate II
  • 2810 Views
  • 5 replies
  • 0 kudos

H7 ADC Gapping - Voids in the digital output

Hardware: H750 Revision VPeripheral in Question: ADC 1 and 3Capture rate: 860HzADC Kernel Clock: 2MhzChannels Converted: 5ADC Conversion overlap: NOTransfer Protocol: DMAADC Conversion Trigger: TIMWe are using ADC 1 and 3 to capture analog pressure s...

0693W00000WJuqEQAT.jpg 0693W00000WJuq9QAD.jpg 0693W00000WJG9yQAH.jpg 0693W00000WJG9jQAH.jpg
PWalt.2 by Associate II
  • 6958 Views
  • 16 replies
  • 0 kudos

regarding storage of values in last two bytes in an array

Hello Folks,I have connected my STML011G4U7 with ISO7816. In my code I am parsing ATR which is an 8 byte array and sending it. Here I need to measure the voltage from ADC which would be (3.3 V) and store it in the last two bytes of an array. How will...

RWagh.2 by Associate II
  • 8948 Views
  • 19 replies
  • 0 kudos

Using external ram as heap space

Hello,I am working on a project with an STM32H753 Microcontroller and I have an external SDRAM 32 mbyte connected to the MCU via FMC. I want to use the SDRAM as default heap space. This because I want cJSON library use this memory space for dynamic a...

SEfte.1 by Associate II
  • 3221 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.