2022-11-29 12:58 PM
hello all,
I want to write a code to test the possibility to use PC13 as output to activate a regulator when the micro is in Vbat mode.. I'm using a STM32F476.
in the manual, in Vbat mode, RTC_OUT still available for Alarm ou wakeup output.
so, in cube Mx I configure RTC in wakeup mode Routed to out. it active PC13 Pin.
I also enable NVIC interrupt.
I use a callback with a toogle on another GPIO to try my code, and it work with this IO.
I enter in the callback every 10sec but nothing append on PC13.
it seem that pc13, RTC and HAL lib have issue together.
if anyone can help me on this please.
I also try to use the PC13 as simple GPIO and it doesnt work until I change some RTC register manualy...
2022-11-29 5:09 PM
> STM32F476
Start with getting a part number right...
2022-11-30 12:01 AM
hello,
I try to test it on a nucleo L476RG where I remove SB17 to disconnect PC13 from user Button and SB45 to disconnect Vbat from VDD.
This is just for test, the target is for a device home made with a STM32L476RGT.
I need to test before finish the pcb.
2022-12-01 1:15 AM
hello @Piranha nothing more about the issue please?
2022-12-01 1:46 AM
Hello @Seth1er ,
Check that timestamp and tamper are disabled.
Imen
2022-12-03 12:26 PM
Check the errata and this one:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.