STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

looking for help with a pwm

I have this code that bring a line up for 5us and down for 20. I want to invert it. I thought the first part of the code was a time base loop and the second was also a timer base loop. but one setting effects the other. If I use htim4.Init.Period = 2...

ulao by Associate III
  • 1547 Views
  • 2 replies
  • 0 kudos

Resolved! Erasing a Flash Page of STM32L4R5 doesn’t work

I'm trying to erase a Flash Page of from my firmware Application with STM32L4R5 using the function 'HAL_FLASHEx_Erase()'. The Application Presence Key is stored in this page. It needs to be erased by the Application to activate the Bootloader (this i...

Shadow by Associate II
  • 3158 Views
  • 2 replies
  • 0 kudos

Not Blinking Ld3 anymore

I use STM32GO1291. when I was debugging I got an error (its picture attached in below ) also my LD3 is not blinking anymore. is microcontroller damaged or there is some other things wrong? why it isn't blinking anymore when I plug!

MFara.4 by Associate III
  • 3757 Views
  • 5 replies
  • 0 kudos

Configuring mems microphone and DFSDM on STM32F769I-eval

I'm having some trouble configurating the DFSDM for reading a mems microphone input on STM32F769I-eval. i've followed the instructions on the application note AN5027 and also the tutorial GETTING STARTED WITH ANALOG. In both cases, the input buffer i...

FNegr.1 by Associate
  • 4080 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F429ZI NUCLEO board that supports 6 SPI interfaces

I'm looking for an ARM based MCU that will handle IC configuration on a board in development. Really just need a full breakout for bench testing. I need it to handle at least 6 SPI lines. Comparing available NUCLEO boards to product selector I found ...

RMas by Associate II
  • 3733 Views
  • 5 replies
  • 0 kudos

Resolved! NUCLEO-U575 board, GPDMA destination address update problem

Hello everybody! So what I want to do, is to update the destination address (DAR) register of the DMA after the last transfer. So I write the desired destination address in a variable "dest_address", then I take the address of that variable and write...

Skfir by Senior
  • 1373 Views
  • 1 replies
  • 0 kudos

Resolved! Disabling memory Read Protection failed

Hello, we have boards with the MCU STM32F746. This works normally but in two cases we had a problem with the option bytes. Several values were changed and now we can't remove the protection.The first board we tried several times to change level prote...

GYacc by Associate II
  • 2901 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.