DMA with complementary pwm STM32F0 ?
HiI want to use DMA with complematry pwm. I am usşng stm32f030 its working only one sample. I have to use stdperiph .Thanks
Ask questions, find answers, and share insights on STM32 products and their technical features.
HiI want to use DMA with complematry pwm. I am usşng stm32f030 its working only one sample. I have to use stdperiph .Thanks
Hello,I've set up FDCAN on my STM32H753. I'm reading the transmissions using both an oscilloscope and an Analog Discovery 2.I'm currently debuggning a loop which transmits the same message over and over again. About half of the times I only get the S...
I am currently implementing communication between STM32G0B1 and STM32H743 using FDCAN.However, I am unable to receive stably. Sometimes it works, sometimes not.Specifically, the following is happening.(G0B1 Recieve)・Data is actually in Fifo, but no r...
Using ADC1 and ADC2 and timer3 trigger rising and falling edges to get a 96KHz event, I understand that we can't use Dual injected simultaneous mode with DMA, so we are using Independent mode, but is there a better (more efficient and robust) mode?I ...
I am coding an STM32G031F8P6. I want to set some interrupt priority values. I am looking at the programming manual, PM0223. In section 4.2 (page 82) Table 25 says that the priority registers NVIC_IPR0-7 are 0xE000E400-0xE000E4EF. That doesn...
Posted on April 19, 2017 at 09:29 Hi all Recently, I created a Win32 application to convert a bitmap (.bmp) file into a header file (.h) in order to display it in mySTM32F746G-DISCO discovery board. Everything works fine but the bitmap (24 bit de...
#include <stdint.h>#define RCC_CFGR_BASE_ADDR 0x40012800UL#define RCC_CFGR_REG_OFFSET 0x04UL#define RCC_CFGR_REG_ADDR (RCC_CFGR_BASE_ADDR + RCC_CFGR_REG_OFFSET )#define RCC_APB2ENR_REG_OFFSET 0x18UL#define RCC_APB2ENR_REG_ADDR (RCC_CFGR_BASE_A...
Hi,I would like to create a new CubeIDE project with a IOC file (from scratch) for B-L475E-IOT01A2 that enables WiFi. I know that there are working examples (for example WiFi_HTTP_Server that works fine) but these projects do not have IOC files. I ha...
Hi,I tried to debug my code into my custom board controller (STM32F030RCT6) through STM32f0 Discovery. when I try to debug, I got the error ''No source available for ''0x8000f24'' So please tell me how to fix this error. Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.