2022-03-31 8:38 PM
I am currently implementing communication between STM32G0B1 and STM32H743 using FDCAN.
However, I am unable to receive stably. Sometimes it works, sometimes not.
Specifically, the following is happening.
(G0B1 Recieve)
・Data is actually in Fifo, but no receive interrupt occurs sometimes.
・Probability of occurrence of no interrupt is around 60%.
The settings are as follows.
(Setting)
・Transmission speed 100khz.
・Transmission mode is classic CAN.
・Filter is set to receive all data.
(Program) ※Created using CubeMx(6.5.0).
・G0B1
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = ENABLE;
hfdcan1.Init.NominalPrescaler = 20;
hfdcan1.Init.NominalSyncJumpWidth = 1;
hfdcan1.Init.NominalTimeSeg1 = 22;
hfdcan1.Init.NominalTimeSeg2 = 2;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 1;
hfdcan1.Init.DataTimeSeg2 = 1;
hfdcan1.Init.StdFiltersNbr = 1;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
・H743
hfdcan2.Instance = FDCAN2;
hfdcan2.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan2.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan2.Init.AutoRetransmission = ENABLE;
hfdcan2.Init.TransmitPause = DISABLE;
hfdcan2.Init.ProtocolException = ENABLE;
hfdcan2.Init.NominalPrescaler = 20;
hfdcan2.Init.NominalSyncJumpWidth = 1;
hfdcan2.Init.NominalTimeSeg1 = 22;
hfdcan2.Init.NominalTimeSeg2 = 2;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 1;
hfdcan1.Init.DataTimeSeg2 = 1;
hfdcan2.Init.MessageRAMOffset = 0;
hfdcan2.Init.StdFiltersNbr = 1;
hfdcan2.Init.ExtFiltersNbr = 0;
hfdcan2.Init.RxFifo0ElmtsNbr = 64;
hfdcan2.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan2.Init.RxFifo1ElmtsNbr = 0;
hfdcan2.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
hfdcan2.Init.TxFifoQueueElmtsNbr = 1;
hfdcan2.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
hfdcan2.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
・Interrupt
HAL_FDCAN_ConfigGlobalFilter(&hfdcan2, FDCAN_REJECT,FDCAN_REJECT, FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE);
HAL_FDCAN_RegisterRxFifo0Callback(&hfdcan2, _RxFifo0Callback);
HAL_FDCAN_RegisterCallback(&hfdcan2, HAL_FDCAN_ERROR_CALLBACK_CB_ID, svErrorCallback);
HAL_FDCAN_RegisterCallback(&hfdcan2, HAL_FDCAN_TX_FIFO_EMPTY_CB_ID, svTxFifoEmptyCallback);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_TX_FIFO_EMPTY, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_RAM_ACCESS_FAILURE, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_ERROR_LOGGING_OVERFLOW, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_RAM_WATCHDOG, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_ARB_PROTOCOL_ERROR, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_DATA_PROTOCOL_ERROR, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_RESERVED_ADDRESS_ACCESS, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_ERROR_PASSIVE, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_ERROR_WARNING, 0);
HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_BUS_OFF, 0);
Best regards.
2022-04-01 2:09 AM
Hello,
2022-04-10 4:56 PM
@Community member
Thanks for the advice.
The H7 and G0 are clocked at 50 MHz and have the same parameters, so the bit rate should not be a problem.So I will try to HSE as source clock.
2022-12-28 7:33 AM
@Haru did ur problem solve after using HSE as source clock.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.