2023-02-06 9:29 PM
void External_Clock_Config(){
TIM_ICInitTypeDef TIM_ICInitStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); //Clock enable
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9| GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(ExternalOSCport, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_2); //alternate func
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_2); //alternate func
TIM_ICInitStructure.TIM_Channel = TIM_Channel_1; //TIM_Channel_3
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Falling;
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStructure.TIM_ICFilter = 0x0;
TIM_ICInit(ExternalOSCTimer, &TIM_ICInitStructure);
NVIC_InitStructure.NVIC_IRQChannel = TIM1_BRK_UP_TRG_COM_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPriority = 0x00;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle ;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;
TIM_OC2Init(TIM1, &TIM_OCInitStructure);
ExternalOSCTimer->CCER |= TIM_CCER_CC2E ;
TIM_OC2PreloadConfig(TIM1, TIM_OCPreload_Disable);
TIM1->CR2 &= (uint16_t)(~(TIM_CR1_DIR | TIM_CR1_CMS | TIM_CR1_CKD));
TIM1->CR2 &= 0XFF7F;
TIM1->ARR = 0xFFFFFFFF;
TIM1->PSC = 0x0000; //set prescale value
TIM1->SMCR |= (uint16_t)(TIM_TS_TI1FP1 | TIM_SMCR_SMS); // external mode 1
TIM_ITConfig(TIM1, TIM_IT_Update, DISABLE);
TIM1->CR1 &= (uint16_t)(~((uint16_t)TIM_CR1_CEN)); //disable timer counting
TIM1->CR1 |= (uint16_t)TIM_CR1_URS; //disable timer counting
NVIC_EnableIRQ(TIM1_CC_IRQn);
}
void TIM1_BRK_UP_TRG_COM_IRQHandler(){ /*OverFlow interrupt **/
if(TIM_GetITStatus(TIM1,TIM_IT_Update) != RESET){
UPEventCount++ ;
if(.UPEventCount == .DelayloopCount){
capture = TIM1->CCR2 ;
TIM1->CCR2 = capture + DelayOverFlow ;
TIM1->DIER |= TIM_IT_CC2;
}
}
void TIM1_CC_IRQHandler(){
if (TIM_GetITStatus(TIM1, TIM_IT_CC2) != RESET){
TIM_ClearITPendingBit(TIM1, TIM_IT_CC2 );
TIM1->DIER &= (uint16_t)~TIM_IT_CC2; }
}Hello
I use stm32f0. I want to generete interrupt when UPEventCount == DelayloopCount(line 65) then, TIM_IT_CCR2 interrupt must be occur when CNT = my value. But CCR2 interrupt occur before CNT not reach my value. But it happens(line 73) when I enable interrupt but not when CCR2 reaches CNT value
In short, this is my expectation that the interrupt will be enabled when it reaches a certain overflow number, and then the caputure compare interrupt will occur when it reaches the specified CNT value.
I haven't figured it out for a long time and I really need help :(
Thanks for now..
@Community member @Community member
jsaun
2023-02-07 3:49 AM
Clear the respective interrupt flag (TIM1->SR.CC2IF) just before you enable the CC2 interrupt.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.