STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EXTI interruption flags

Hi.I am having some issues trying to use the EXTI module, to implement interruption routines associated to ports.The problem is related to the behavior of STM32 microcontrollers with ports interruptions. In most microcontrollers (i.e. Texas Instrumen...

JNava.1 by Associate II
  • 10211 Views
  • 13 replies
  • 0 kudos

Resolved! If I want to control a relay via the TX of a UART do I just connect the appropriate STM32 pin to the relay? Or is there anything else I need to do (besides programming)?

I'm looking to use a ITS4200S-ME-P relay to switch a high voltage signal and would like to control that via a UART. Per the datasheet this relay, "can be switched on and off with standard logic ground related logic signal at pin IN."

DMill.16 by Associate II
  • 4170 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G4: ADC sampling and hold capacitor value

SetupSTM32G491KEADC1 Input Channel 3 using Pin PA2Vdd = 3VRC-Filter at the ADC input with R = 33 Ohm, C = 330 pFObservationWhen measuring the voltage at the ADC input with an oscilloscope, we see the voltage drop caused by switching the input signal ...

tssh by Associate
  • 7947 Views
  • 4 replies
  • 3 kudos

Resolved! Executing main() by XIP with W25Q32 QSPI Flash

HiI'm using STM32H750VBT6 with W25Q32 QSPI external flash memory from Winbond and I'm using Keil Microvision IDE with ARM_CC Compiler.I'm trying to execute my whole project from the QSPI flash directly (which is called XIP). I know that I have to con...

Farbod by Associate
  • 2896 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 Internal Flash erase but not 0xFF or 0x00

Hello. I am working with internal Flash memory on STM32F407, I have 4 functions as described below:void FLASH_save_CP_serial(uint32_t serial_number) {     taskENTER_CRITICAL();     uint32_t write_test = 12345;     FLASH_EraseInitTypeDef Eras...

LPetr.1 by Senior II
  • 3077 Views
  • 2 replies
  • 1 kudos

How get lowest sleep current in STM32F30.

Hi All,I am using STM32F301k8 for my remote project. I am using HSI clock source, I am enable one i/o interrupt and using UART1. for sleep i am using STOP mode by following functions.HAL_UART_DeInit(&huart1);   __HAL_RCC_USART1_CLK_DISABLE();HAL_Susp...

nraj by Associate II
  • 2138 Views
  • 4 replies
  • 1 kudos

Resolved! {RESOLVED] STM32F0, why my PLL makes trouble?

STM32F070RB stepping Y, with a 24MHz crystal as HSE. No LSE.In the Cube, enabled PLL sourced from the HSE; SYSCLK goes to 48 MHz.Then, as soon as I run thru HAL_RCC_OscConfig, debugger loses connection and I don't know what the chip does.​So I've swi...

Pavel A. by Super User
  • 2434 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.