2023-02-17 9:39 AM
We have a project which reads CAN data on both FDCAN ports. Bitrate 500 kBit is working perfectly, but with 1 MBit no data can be read.
PIN-Speed = HIGH (also tried MEDIUM and VERY_HIGH, but no change)
CAN-Clock = 80 MHz
We already tried CAN Bittiming parameters with different Sampling points (56% ... 90%)
CAN-Signals look perfect on the scope.
When debugging the Flag in the LastErrorCode Bit of ProtocolStatusRegister is set to 2 (=Form error).
With PEAK-Diag FD the signal can be read ok, Bus Termination Resistor is ok (60 Ohms).
Currently we have no idea, what might the reason for the problem.
Any comments are very much appreciated!
BR GS
Solved! Go to Solution.
2023-02-17 10:31 AM
Ok, we exchanged the board by another one, and that one works. Currently we can not say, why the first one won't read 1 MBit.
2023-02-17 10:31 AM
Ok, we exchanged the board by another one, and that one works. Currently we can not say, why the first one won't read 1 MBit.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.