STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Change Uart baud rate on the fly with cube?

Posted on September 18, 2017 at 16:07I see that this has been asked a few times with no real resolution or workaround, so I'll ask again please?I have USART3 configured at 9600 Baud. I test this with a terminal program also set at 9600 and it works ...

nibbly78 by Associate III
  • 4629 Views
  • 8 replies
  • 1 kudos

STM32H750IBK6 REV V sample what is max FMC CLK we can run SDRAM the datasheet says 2 different values for rev V and REV Y IC revision what is safe area of operating FMC CLK with SDRAM

STM32H750IBK6 REV V sample what is max FMC CLK we can run SDRAMthe datasheet says 2 different values for rev V and REV Y IC revision what is safe area of operating FMC CLK with SDRAM

Ssaga.1 by Associate II
  • 4219 Views
  • 7 replies
  • 0 kudos

bno055 with stm32

I wanted to see if the bno055 sensor is ready and set the PB8, PB9 pins as SDA, SCL. (my mcu = stm32f334r8)connectionsSDA_pin -> SDA pin sensorSCL_pin -> SCL pin sensorVCC -> VCCGND -> GNDbut the variable is never HAL_OKthanks for answer.

0693W00000aI7CEQA0.png
Loodan22 by Associate II
  • 6733 Views
  • 8 replies
  • 0 kudos

Timers wont fire interrupt but normal gpio interrupt works

I have configured a timer to trigger on a rising edge of my signal so that I can measure the period of my signal. I tried the basic gpio interrupts and it worked fine, but when I tried it with the timer interrupt, the callback was never called, as if...

MSadf.1 by Associate II
  • 4227 Views
  • 9 replies
  • 0 kudos

How to know why a thread doesn't start?

I have a thread that doesn't start. The thread is created with autostart and the function return successfully, but the thread doesn't start...I don't know why. What instrument of debugging are available to go deeper in this issue?

IVent.1 by Senior
  • 1478 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.