STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32C0316-DK RTC reset after reboot.

I am using STM32C0316-DK and testing RTC.LSE is used for RTC Clock.I removed the code setting rtc time/date in MX_RTC_Init(). After change the time/date, reboot board but rtc time/date are cleared.When I checked RTC_CR register, it was also cleared. ...

hcho.2 by Associate
  • 2266 Views
  • 4 replies
  • 0 kudos

Resolved! Problem with external loader for a H7-device and Octo SPI

I have a custom board with STM32H725IG using a multiplexed Octo SPI memory S71KL256xx. I have managed to establish reasonable communication to the memory thanks to example given in AN5050 even tough it was not H7. Sometimes, however, there are read/w...

Resolved! STM32H7 FDCAN 8 Mbit/s setup / docum. unclear SYNC_SEG

Heyho,I don't get the FDCAN on a STM32H735g-DK working with 8 Mbit/s.I feed the FDCANs with 80 MHz so that the "time quantum" is 12.5 ns to make 8 Mbit possible with the integers.I use the recommended kvaser website for calculations:https://www.kvase...

LCE by Principal II
  • 14367 Views
  • 26 replies
  • 0 kudos

I am trying to read several adc channels on the stm32 microcontroller, but it won't let me, it only reads the first one.

I am trying to read several adc channels on the stm32 microcontroller, but it won't let me, it only reads the first one. I have seen in the registers that when changing channel what it does is that it sets the selected channel bit to 1 and does not m...

lroca.2 by Associate
  • 1436 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.