2023-02-27 8:48 AM
Heyho,
I don't get the FDCAN on a STM32H735g-DK working with 8 Mbit/s.
I feed the FDCANs with 80 MHz so that the "time quantum" is 12.5 ns to make 8 Mbit possible with the integers.
I use the recommended kvaser website for calculations:
https://www.kvaser.com/support/calculators/can-fd-bit-timing-calculator/#/canfd
/* clock / timing */
/* nominal = arbitration phase
* NBTP
* 80 MHz: tq = NominalPrescaler x (1/fdcan_ker_ck)
* -> tq = 12.5 ns
* data rate = 1 / ((SyncSeg + Seg1 + Seg2) * tq)
* with SyncSeg = 1
* 0.5 Mbps = 160 * tq
* -> TimeSeg1 + TimeSeg2 = 159
*/
phCan->Init.NominalPrescaler = 1; /* tq = NominalPrescaler x (1/fdcan_ker_ck) */
#if( 1 )
/* 5000 ppm */
phCan->Init.NominalTimeSeg1 = 138; /* NTSEG1 1..256, NominalTimeSeg1 = Propagation_segment + Phase_segment_1 */
phCan->Init.NominalTimeSeg2 = 21; /* NTSEG2 1..128 */
phCan->Init.NominalSyncJumpWidth = 20; /* NSJW 1..128 should be < NTSEG2 */
#else
/* 500 ppm */
phCan->Init.NominalTimeSeg1 = 153; /* NTSEG1 1..256, NominalTimeSeg1 = Propagation_segment + Phase_segment_1 */
phCan->Init.NominalTimeSeg2 = 6; /* NTSEG2 1..128 */
phCan->Init.NominalSyncJumpWidth = 3; /* NSJW 1..128 should be < NTSEG2 */
#endif
/* data = data phase with bit rate switching
* DBTP
* 80 MHz: tq = DataPrescaler x (1/fdcan_ker_ck)
* -> tq = 12.5 ns
* data rate = 1 / ((SyncSeg + Seg1 + Seg2) * tq)
* with SyncSeg = 1
*/
phCan->Init.DataPrescaler = 1; /* DBRP 1..32 */
#if CAN_FD_DATA_8MB
/* 8 Mbps = 10 * tq
* -> TimeSeg1 + TimeSeg2 = 9
*/
phCan->Init.DataTimeSeg1 = 5; /* NTSEG1 1..32, NominalTimeSeg1 = Propagation_segment + Phase_segment_1 */
phCan->Init.DataTimeSeg2 = 4; /* NTSEG2 1..16 */
phCan->Init.DataSyncJumpWidth = 4; /* NSJW 1..16 should be < NTSEG2 */
#else
/* 2 Mbps = 40 * tq
* -> TimeSeg1 + TimeSeg2 = 39
*/
phCan->Init.DataTimeSeg1 = 24; /* NTSEG1 1..32, NominalTimeSeg1 = Propagation_segment + Phase_segment_1 */
phCan->Init.DataTimeSeg2 = 15; /* NTSEG2 1..16 */
phCan->Init.DataSyncJumpWidth = 14; /* NSJW 1..16 should be < NTSEG2 */
#endif0.5 Mbit in arbitration phase is working (checked bit rate on scope), so is data rate of 2 Mbit/s (checked bit rate on scope).
When using the 8 Mbit settings, the peripheral "hangs" after the first output, which doen's show any sign of BSR / 8 Mbit.
Any ideas?
Or even better any examples how to get to 8 Mbit/s ?
Solved! Go to Solution.
2023-03-16 11:22 AM
What are you doing with transmitter delay compensation? Surely things get a lot tighter when looking for signals coming back at higher speeds.
Check also status/error flagging in these conditions.
HAL_FDCAN_ConfigTxDelayCompensation : Configure the transmitter delay HAL_FDCAN_EnableTxDelayCompensation : Enable the transmitter delay compensation
https://community.st.com/s/question/0D53W00000AZ8prSAD/can-fd-error-status
2023-02-27 10:31 PM
I just checked the register values again and they were wrong, so above are the "correct" values.
Still the same problem:
2 Mbps perfect,
8 Mbps not working
Any ideas?
Is the input clock fdcan_ker_ck = 80 MHz too low?
Shouldn't be, ST's 2 Mbps examples use 20 MHz, and at VOS1 max FDCAN clock is 100 MHz.
Edit: 4 Mbps is working with:
DBRP = 1
DTSEG1 = 12
DTSEG2 = 7
DSJW = 5
2023-02-27 11:04 PM
Documentation, RM0468, latest edition:
61.4.4 Bit timing, pg. 2528
Synchronization segment (SYNC_SEG): a bit change is expected to occur within this
time segment, that has a fixed length of one time quantum (1 x tq).
DBTP reg description, page 2567:
Therefore the length of the bit time is (DTSEG1 + DTSEG2 + 3) tq for programmed values
Same descr. in NBTP.
So, which one is correct, or are these 2 different things?
@Imen DAHMEN please?
Edit: Same in G4 RM
2023-02-28 8:05 AM
Anybody getting 8 Mbps on a H735 ?
At least someone from @ ST ever got that working?
I tried all kinds of timings, and I can't imagine that the CCU is needed, especially when communicating only with another on-chip FDCAN with the same timing settings.
Or this the problem, trying to have 2 FDCANs running with 8 Mbps at the same time?
2023-02-28 8:36 AM
This is almost funny...
When I set FDCAN1 Mode to FDCAN_MODE_EXTERNAL_LOOPBACK, it sends with 8 Mbps, and FDCAN2 receives data correctly.
When I set FDCAN2 back to FDCAN_MODE_NORMAL, no 8 Mbps on the scope, no Rx on FDCAN2.
Then I get in FDCAN1:
PSR = 0000050F
TDVC = 0 mtq
PXE = 0
REDL = 0
RBRS = 0
RESI = 0
DLEC = 05 -> error: bit 0
BO = 0
EW = 0
EP = 0
ACT = 01 idle
LEC = 07 -> error: no change
ECR = 00010008
CEL = 1 CAN error log
RP = 0
REC = 0 RX err
TEC = 8 TX err
2023-03-01 3:16 AM
8 Mbit still not working (except ext loopback).
Checked again RM and DS, no specs concerning data rate.
Anybody?
@Peter BENSCH maybe?
2023-03-01 9:25 AM
@Community member Thank you for your trust, but for once, due to lack of experience, I have nothing to contribute here.
Regards
/Peter
2023-03-01 11:10 PM
@Peter BENSCH Thanks for your reply, at least something! :)
Maybe you can forward this question to your FDCAN experts?
It's really strange, everthing working fine up to 4 Mbit/s on both peripherals, but as I described: 8 Mbit works only in external loopback mode.
2023-03-02 1:02 AM
Hello @LCE (Community Member) ,
Thank you for your contribution.
I will escalate this issue internally to the FDCAN experts and I'll make sure to post more details here as soon as I hear back from our team.
Imen
2023-03-02 1:21 AM
@Imen DAHMEN
Thanks!
Anyway, note the documentation bug in DBTP and NBTP registers.
I'm pretty sure now that the +1 for the bit time is the correct value (instead of the +3).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.