2023-03-17 9:11 AM
I am using stm32-g07 and I managed to generate two waves: one reference and another phase shifted. Now I want to calculate the phase shift between the two. I tried two options:
However, in both cases, I don't get the index for the highest peak because I am using a phase accumulator and based on the phase increment, the peak value is constantly fluctuating. How to solve this problem?
The code is a bit mess because i was trying different methods. But my sine wave generation is here : void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
[Code in comment below]
2023-03-17 9:13 AM
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2023 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stdlib.h"
#include "math.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define PI 3.14159
#define NS 4096
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
DAC_HandleTypeDef hdac1;
TIM_HandleTypeDef htim16;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
uint32_t Fs = 0;
uint64_t f_exp = 1000; //
uint64_t tuning = 0;
uint32_t idx = 0;
int output_val1 = 0;
int output_val2 = 0;
static int ratio = 0;
int start = 0;
int end = 0;
int phase_diff = 0;
int slow_counter = 0;
int counter = 0;
int n = 0;
float raw = 0;
float adc = 0;
uint32_t phase_diff_t = 0;
uint32_t phase = 0;
uint32_t diff = 0;
int LUT_r[NS];
int LUT_s[NS];
int PSC = 0;
int ARR = 0;
uint64_t Fclk = 64000000;
uint32_t adc_buffer[NS];
int buffer = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_TIM16_Init(void);
static void MX_DAC1_Init(void);
static void MX_ADC1_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* LUT */
//
void sine_val(int x){
if(x == 1){
for(int i = 0;i < NS;i++){
LUT_r[i] = (sin(i* (2*PI)/NS )+1)*(4095/2);
}
}
else{
for(int i = 0;i < NS;i++){
LUT_s[i] = (sin(i* (2*PI)/NS - PI/2)+1)*(4095/2);
}
}
}
void samplingrate(){
Fs = Fclk/((PSC+1) * (ARR+1));
}
void phase_increment(int16_t freq_out, uint32_t Fs, uint8_t acc_depth) {
tuning = (round(freq_out * pow(2, acc_depth) / Fs));
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();
MX_TIM16_Init();
MX_DAC1_Init();
MX_ADC1_Init();
/* USER CODE BEGIN 2 */
sine_val(1);
sine_val(2);
PSC = htim16.Init.Prescaler;
ARR = htim16.Init.Period;
samplingrate();
ratio = Fs/f_exp;
phase_increment(f_exp, Fs, 32);
HAL_TIM_Base_Start_IT(&htim16);
HAL_ADC_Start(&hadc1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
// HAL_ADC_PollForConversion(&hadc1, 0.001);
//HAL_ADC_GetValue(&hadc1)
raw = output_val1 * 3.3/4096;
if(raw > 3.29){
counter++;
start = idx - start;
}
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 4 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
// Check which version of the timer triggered this callback and toggle LED
if (htim == &htim16 )
{
phase += tuning;
idx = (phase >> 20) & 0xFFF;
output_val1 = LUT_r[idx];
output_val2 = LUT_s[idx];
if(output_val1 >= 3900){
start = idx;
}
if(output_val2 >= 4000){
end = idx;
}
HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, output_val1);
HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_2, DAC_ALIGN_12B_R, output_val2);
//
//
HAL_DAC_Start(&hdac1, DAC_CHANNEL_1);
HAL_DAC_Start(&hdac1, DAC_CHANNEL_2);
}
}
Unfortunately i couldn't post whole code but whatever i wrote for myself is here.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.