STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G030 DMA to GPIO BSRR bus error

HiSTM32G0 series is a newer chip family with more advanced DMA/MUX to provide more flexibility.my code, which uses tim16 update to request DMA to transfer from memory to GPIO BSRR. The code works on STM32F030 but fail in G030. The request from TIM...

STM32F732 BOOT1 pin

I thought the BOOT Modes used BOOT0 & BOOT1(PB2) pinsand to pull BOOT0 (high) and BOOT1(low) to get BOOT MODE (SYSTEM MEMORY) and allow the STM32CUDE programmer!I've looked thru the STM32F723 Docs and PB2 does not seem to show/sharethe BOOT1 pin func...

CTerr.1 by Associate II
  • 4281 Views
  • 5 replies
  • 0 kudos

Single bank mode for STM32L471RxE devices

Hi EveryoneI'm having some trouble with the reference manuals description of single bank mode for the STM32L471RxE devices. In the attachments you can see that the page number for bank 2 always starts with 256, regardless of the flash size. What I co...

0693W00000aJa7GQAS.png 0693W00000aJaEzQAK.png
DWyde.1 by Associate II
  • 2542 Views
  • 4 replies
  • 0 kudos

Unwanted NMI interrupt of CSS peripheral of stm32G491CC

Good morning community,I am contacting you to ask for support regarding a EMC immunity problem I'm experiencing.My application uses an stm32g491cc MCU with an external 8 MHz ceramic resonator (HSE)What i observe is a reset of the microcontroller duri...

GIabi.1 by Associate II
  • 2286 Views
  • 0 replies
  • 0 kudos

STM32C0 Boot Programming

Hi, I am planning to use STM32C011F6 for a simple application and want to download application through UART1. How to use BOOT0 pin to program MCU for the first time. According to data sheet, UART1 pins PA9/PA10 needs remapping to function as UART. Al...

KGane.1 by Associate III
  • 2013 Views
  • 1 replies
  • 0 kudos

Resolved! [ STM32G070 ] STM32G070 input mode pin speed setting?

Dear Sir,​In STM32G070 series, the code shows the speed setting for GPIO output,If my GPIO is setting for input to receive external interrupt, does the speed setting also apply for GPIO input mode?Thanks/** @defgroup GPIO_speed GPIO speed * @brief ...

E-John by Associate III
  • 2579 Views
  • 2 replies
  • 1 kudos

SDIO API for H7

Sorry, I am new STM32 MCU :grinning_face_with_sweat: ​I want to bring up WIFI function with SDIO to connect Internet, but I cannot find any SDIO API in H7 like stm32f4xx_sdio.c.The link is where I can find the answer I want, but it only supports H747...

wG.1 by Associate II
  • 2014 Views
  • 1 replies
  • 0 kudos

STM32F407VGTX_FLASH.ld: No such file or directory error

Hi i wanted to try new extension but i get this error. The code is a basic blink its working on cubeide but when i try on vscode this happens.Thank you already[build] c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltoo...

HSarı.1 by Associate
  • 4389 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.