2023-03-23 10:58 PM
Hi, I am planning to use STM32C011F6 for a simple application and want to download application through UART1. How to use BOOT0 pin to program MCU for the first time.
According to data sheet, UART1 pins PA9/PA10 needs remapping to function as UART. Also the default functionality of PA14-BOOT0 is SWD interface SWCLK.
How to program MCU for the first time without using SWD interface?
2023-03-24 12:32 AM
The latest (Rev 57) AN2606 Application note "STM32 microcontroller system memory boot mode" has a C0 chapter stating
"Note:On WLCSP12, SO8N, TSSOP20 and UFQFN20 packages USART1 PA9/PA10 IOs are remapped on PA11/PA12."
Haven't tried it, though.
hth
KnarfB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.