STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

hcan1 not working while hcan2 does work with same settings

I'm working with a custom STM32F105 board with two similar CAN circuits but CAN1 is not working.I use STM32 HAL with this custom CAN lib which handles configuration and buffering.It was working before with the same hardware but I can't get it woking ...

MEige.1 by Associate III
  • 1745 Views
  • 2 replies
  • 0 kudos

CAN bus not responding at 1Mbps bit rate

I'm using STM32F446RC controller CAN BUS 1. Trying to operate CAN BUS at 1mbps speed when using 100kbps bit rate it is working fine but not at 1Mbps bit rate. Is there any solution for this.

TES.1 by Associate II
  • 7609 Views
  • 12 replies
  • 0 kudos

Nucleo-G070RB prints garbage via UART

I've programmed this board to print out some data via the onboard serial interface (using UART2). But all I get is garbage characters, and I can't figure out why. I checked the baud rate of both the Nucleo and the terminal, I've tried different termi...

0693W00000GZtokQAD.png
BSerb by Associate II
  • 1667 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.