STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FMC vs FSMC

Hello,A product I'm working on requires communicating with an FPGA over an 8 bit data + 24 bit address bus.To support a legacy design with the least possible changes I need the bus to toggle at 43.75 MHz.All I need is single (non-burst) address acces...

skon.1 by Senior
  • 5385 Views
  • 3 replies
  • 0 kudos

Resolved! stm32f446re gpio as active LOW reset pin

im using pc8 as a reset pin and ive check it with a logic analyzer and wen its initalized it drops low then goes back to high before im calling my function to drop it low btw im using saleae logic 2 void reset_pin_init(void){ //PC8 RCC->AHB1ENR |= ...

Cannot find a single STM32H7 series chip at any of the standard sellers in North America while the STM32MP series can be found anywhere, so my question is;What does support, in terms of manufacturing, of the STM32H7 look like in the future?

I refuse to purchase a $40 chip for over $400 dollars so will not purchase on current market. I based an entire product line on the STM32H757 and now I cannot buy them so the real question is, should I move to a different processor?

rwareinc by Associate III
  • 5723 Views
  • 11 replies
  • 0 kudos

Resolved! Implementing w5500 to stm32l431rct6

Hi everyoneI'm a student and I'm totally new to stm32 controllersI spend two weeks trying connecting stm32l431rct6 to w5500 but I failedcan any one guide me to a tutorial or some videos that I can use ? or can anyone help methank you

Abdegou_8 by Associate II
  • 5482 Views
  • 2 replies
  • 0 kudos

Resolved! STM32h743 max FMC SDRAM clock 100MHz?

Hi,I found this in datasheet But we config SDRAM at 120MHz, because we are running at 480MHz.(480MHz / 2 / 2 = 120MHz).I am thinking the datasheet is for STM32H7xx 400MHz, because when I config SDRAM at 120MHz, the system works fine without issue.Doe...

_legacyfs_online_stmicro_images_0693W00000bhavNQAQ.png
Dat Tran by Senior II
  • 2838 Views
  • 3 replies
  • 0 kudos

STM32F407VE sector 4 erase problems

I made a mistake a few days ago that resulted in my program erasing part of itself. \\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\\I'm doing a bare metal bootloader on a STM32F407VE and ha...

BKuhn by Associate III
  • 2713 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.