2023-04-11 12:22 AM
When configuring UART2 in the STM32C0316-DK, the emulator is locked.
Error in executing 'step' command ...
Target is not responding, retrying...
Code is running here (stm32c0xx_hal_msp.c line 272):
/**USART2 GPIO Configuration
PA8 ------> USART2_TX
PA13 ------> USART2_RX
*/
GPIO_InitStruct.Pin = GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF1_USART2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF4_USART2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
Need you help.
Tim
Solved! Go to Solution.
2023-04-11 12:36 AM
Hello @tpeng.1 ,
this is quite common mistake, you reconfigured one of your pins used for debug (PA13). You should use other pins for the USART2, when you want to use SWD.
BR,
Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-11 12:36 AM
Hello @tpeng.1 ,
this is quite common mistake, you reconfigured one of your pins used for debug (PA13). You should use other pins for the USART2, when you want to use SWD.
BR,
Jaroslav
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-11 12:57 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.