STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! External crystal on STM32F303CCT6

Hello all, I don't know why but my MCU STM32F303CCT6 don't work with external crystal, below schematics:The used crystal is ABM3B-8.000MHZ-10-1-U-T with load capacitors 10pF. Later I find in STM Datasheet that I should use resistor on OSC32_OUT pin. ...

_legacyfs_online_stmicro_images_0693W00000bkpe2QAA.png
MSzła.1 by Associate III
  • 4299 Views
  • 6 replies
  • 0 kudos

How do I transmit data via UART, which is not connected to the ST-LINK to a Windows computer? Which drivers are needed?

This question uses the STM32H723So I am transmitting data at 7MB/s over UART to a PC. Currently, it uses UART3, which is connected to the ST-LINK. When I view the data on the Windows PC it is fine but every now and then the received data is wrong, an...

_legacyfs_online_stmicro_images_0693W00000bkrHyQAI.png
KSOdin2 by Associate III
  • 3970 Views
  • 3 replies
  • 0 kudos

Bug in HAL STM32C011J6M6 when MCO Output is set.

Hello,I have a very simple project to generate 50/60Hz PWM signal with MCO 3MHz output for other HW. So far my code is just turning on the PWM, everything else is generated by CubeMX. But the MCU falls into HardFault when MCO (Pin 4 PF2-NRST) is set ...

ONadr.1 by Senior III
  • 5424 Views
  • 7 replies
  • 0 kudos

Resolved! Implementing APS12808L-3OBM HyperRam in Memory Mapped Mode on STM32H725. Does anyone have a working configuration?

I'm implementing a custom board with an APS12808L-3OBM HyperRam in Memory Mapped Mode on STM32H725, as recommended by ST to replace the S70KL1281 memory.I'm having some problems getting the ram to respond. This is my current configuration:static void...

MLuis.1 by Associate III
  • 2363 Views
  • 1 replies
  • 0 kudos

What are the potential reasons for Hardfault?

I have a custom board with a basic crystal oscillator connected to the High Speed Oscillator pins of my STM32F446RET6. I assembled 2 boards and found out only 1 board works fine but the other does not. I replaced the crystal and the capacitors but I ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.