STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 installer for Windows 11

I'm setting up a new computer. I tried to download STM32 installer for windows 11 from this page https://www.openstm32.org/Downloading%2Bthe%2BSystem%2BWorkbench%2Bfor%2BSTM32%2Binstaller, but it kept saying install_sw4stm32_win_64bits-v2.9.exe canno...

LKa.1 by Associate
  • 4630 Views
  • 0 replies
  • 0 kudos

Resolved! How to set the Prescaler register?

Hi there,​I am using Nucleo-H745ZI-Q. I am trying to create 1 microsecond(us) timer. My timer clock frequency is 75Mhz. So first time, I put in 75Mhz for the prescaler. But the error range was 500 ms per second. So I googled and found this comment. ...

SKang.11 by Associate
  • 4013 Views
  • 2 replies
  • 0 kudos

Resolved! How to get started with the STM32H747I discovery board

The firmware that is delivered on the board has an evaluation tools link that is broken:"/en/evaluation-tools/DISCO-H747XI.html"and going through the user manual and powering on the board does not start the demo examples.Where can I find a getting st...

BillG by Associate II
  • 2353 Views
  • 2 replies
  • 0 kudos

Garbage values while using multiple ADC channels

Hi,I am using STM32H743 Nucleo to interface 9 analog sensors on different ADC channels of ADC1. ADC1 is configured as:hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV6; hadc1.Init.Resolution = ADC_RESOLUTION_16B; hadc1.Init.Scan...

RJain.1 by Associate III
  • 1261 Views
  • 1 replies
  • 0 kudos

Resolved! program hangs after using SPI_TransmitReceive_DMA

My program hangs after the return statement. pDataDMA = pData->data(); HAL_StatusTypeDef val = HAL_SPI_TransmitReceive_DMA(&spih, pDataDMA, pDataDMA, pData->size()); if (val != HAL_OK) { Error_Handler(); } ...

Dvan .8 by Associate II
  • 1290 Views
  • 1 replies
  • 0 kudos

Noise due data transmission using UART on STM32L476RE

In my project, I'm using the STM32L476RELQFP64 microcontroller to process data from an external ADC that communicates via SPI. The objective is to transmit this processed data to a display using UART. However, I'm facing difficulties with the data tr...

LRosa.1 by Associate
  • 1594 Views
  • 0 replies
  • 1 kudos

My I2C communication in DMA mode is not working properly

Hello, I have developed two codes to test the I2C communication between a master device (STM32F411RE) and a slave device (also STM32F411RE) in DMA mode. The expected result is as follows: whenever there is a rising or falling edge interruption on GPI...

Mabou.1 by Associate II
  • 3907 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.