STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F411 Flash programming returns PGA & PGS Error

I'm trying to program some data into a flash sector but the HAL_FLASH_PROGRAM returnsa value of 10 which maps to pga and pgs error.HAL_FLASH_Unlock(); uint64_t val = (uint64_t)(data->at(i) << 8 | data->at(i + 1) << 8 | data...

Dvan .8 by Associate II
  • 872 Views
  • 0 replies
  • 0 kudos

Hi everyone, I am using STM32F411re for a project and I I have to define I2C communication. Below I am will mention the both cpp and header file and the error I got while compiling the code.

Header file: /** * @file I2CCommunication.h * @brief Header file for controlling I2C messages */ #ifndef INC_I2CCOMMUNICATION_H_ #define INC_I2CCOMMUNICATION_H_ #include "DefaultDefines.h" /** * @brief The I2CCommunication class * * This ...

Kanan by Associate
  • 1308 Views
  • 0 replies
  • 0 kudos

ADC1 + ADC3 for measure analog signal

Hello,I have successfully setup ADC3 to measure values on channels PC2_C, PC3_C, temperature, ... on STM32H753ZIT6And now I want to add ADC1 to measure other channels. But the program waits for the LL_ADC_IsActiveFlag_ADRDY flag. My init function for...

STM32L452 Can't read ADC after WakeUp from deepsleep

In previous time we were using STM32L412RCT6 to do the ADC working, where no problem and work fine, When we have flash memory short, we were decided to migrate to STM32L452RET6 (pin to pin compatible), The issue has occurred, the ADC working fine w...

DShih.1 by Associate II
  • 1964 Views
  • 3 replies
  • 0 kudos

MotionAC and STM32L073

Good day.I wanted to know why the MotionAC library is not supported on the STM32L073 MCU. And is support planned in the future?

ASadk.1 by Associate
  • 671 Views
  • 0 replies
  • 0 kudos

Resolved! How to configure CAN filters to use CAN1 and CAN2 parallelly.

Both CAN buses are transmitting correctly. But when I initialize CAN1 and CAN2 only CAN2 receives messages, when only CAN2 is initialized it receives. same for the CAN1. Here I attached my initializing function. static void MX_CAN1_Init(void) { ...

SPeri.1 by Associate II
  • 8682 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.