2023-05-29 10:34 AM
2023-05-29 11:03 AM
I am using the Nucleo F303ze board, 3 differential channels on ADC 1 and 3 differential channels on ADC 3. I will use DMA in normal mode and Timer 20 to trigger both ADC1 and ADC3 .
I am using STM32CudeIDE 1.12.1.
Regarding the DMA:
For ADC1 : DMA1 channel 1 global interrupt enabled
For ADC3: DMA2 channel 5 global interrupt enabled
I dont know if the following should solve my problem.
I have the following setup for my code in the while(1) loop and wondering how to determine when both DMA1 channel 1 and DMA2 channels have been filled to stop:
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adcResultsDMA1, 3 *2048);
HAL_ADC_Start_DMA(&hadc3, (uint32_t*)adcResultsDMA3, 3 * 2048);
HAL_TIM_Base_Start(&htim20);
/ *** Code required to determine when DMA completed for both ADC1 and ADC3 ****/
// ADC DMA complete ISR exited
HAL_ADC_Stop_DMA(&hadc1);
HAL_ADC_Stop_DMA(&hadc3);
HAL_TIM_Base_Stop(&htim20);
Thanks
David Nyarko
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.