STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Functional safety

Hello,I would like to receive the UL(E480533) condition of acceptability what is the failures in the internal watchdog? is external watchdog is needed ?Do you have risk assessment for STM32F ? can you share it?can you recommend a consulting company t...

yeila.1 by Associate
  • 1082 Views
  • 1 replies
  • 0 kudos

Higher priority timer will preempt lower priority external interrupt, but will not preempt a lower priority timer.

EDIT: Hello, everyone. My code issue seems to have resolved itself after much changing, but I never did find out what was happening. My real question was answered: There are no likely circumstances that a higher-priority interrupt should not pre-e...

Charles P by Associate II
  • 7899 Views
  • 14 replies
  • 0 kudos

I2C communication address issue

Hi, All. I have come across an odd situation in I2C communication between F405 and sensors1) F405 is master. address is 7 Bit2) with 3 slave I2C sensors , address, 22h,35h,78h3) There is no issue to read data from sensors of 22h and 35hbut when comm...

_legacyfs_online_stmicro_images_0693W00000bkmxQQAQ.png _legacyfs_online_stmicro_images_0693W00000bkmxaQAA.png
Forest.Xu by Associate II
  • 2336 Views
  • 3 replies
  • 0 kudos

Resolved! Making a UART frame from ADC value WITH ASCII Control Character

Hello,My aim is to send (from my nucleo board_F103+FTDI) somes ADC value from DMA.Easy...But i would like a frame like that (Windows Software need it):<STX>ADC1;ADC2;ADC3<ETX><CR><LF>I'm able to send data, no more...uint16_t sensor_B =1234; char str[...

jlecl.1 by Associate III
  • 1785 Views
  • 2 replies
  • 0 kudos

Resolved! Data transmit by UARD (DMA) with junk character

Dear eveyone,I' little confuse..I'm trying to send dat over uart from a nucleo board (F103 + FDTI). If a use "normal"method, it's work great.I mean, i receive "1234567890" WITH a new line.uint8_t start [20]= "1234567890 \n\r"; HAL_UART_Transmit(&huar...

jlecl.1 by Associate III
  • 2496 Views
  • 4 replies
  • 0 kudos

Resolved! Delaying the reset that comes from the NRST

Hi all,I'm using STM32L562VETQmy question is:can i delay the reset for about 20ms when pressing the NRST pin ?i want to give LED-Indication for the device reset.in other words, can the reset -that comes from the NRST pin- be delayed for a specific am...

_legacyfs_online_stmicro_images_0693W00000bl9zFQAQ.png
WAdel.1 by Associate II
  • 3715 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.