2023-05-30 5:54 AM
Header file:
/**
* @file I2CCommunication.h
* @brief Header file for controlling I2C messages
*/
#ifndef INC_I2CCOMMUNICATION_H_
#define INC_I2CCOMMUNICATION_H_
#include "DefaultDefines.h"
/**
* @brief The I2CCommunication class
*
* This class will handle the sending and receiving of messages over I2C
*/
class I2CCommunication {
public:
I2CCommunication(I2C_HandleTypeDef _hi2c);
virtual ~I2CCommunication() = default;
HAL_StatusTypeDef i2cWrite8(uint8_t, uint8_t);
HAL_StatusTypeDef i2cRead8(uint8_t, uint8_t, uint8_t*);
HAL_StatusTypeDef i2cRead16(uint8_t, uint8_t, uint16_t*);
private:
I2C_HandleTypeDef mI2CHandle;
};
#endif /* INC_I2CCOMMUNICATION_H_ */CPP file:
/**
* @file I2CCommunication.cpp
* @brief Source file for the wrapper over the HAL_i2c functions
*/
#include <I2CCommunication.h>
/**
* @brief Constructor for I2CCommunication
* @param[in] I2C_HandleTypeDef _hi2c The handle for the HAL I2C communication
* @retval None
*/
I2CCommunication::I2CCommunication(I2C_HandleTypeDef _hi2c) {
mI2CHandle = _hi2c;
}
/**
* @brief Send one byte over I2C
* @param[in] uint8_t address The address of the I2C slave
* @param[in] uint8_t msg The message for the I2C slave
* @retval HAL_StatusTypeDef The status of the HAL functions that are called within this method
*
* This method will call the HAL_I2C function to send an 8 bit message over I2C
*/
HAL_StatusTypeDef I2CCommunication::i2cWrite8(uint8_t _address, uint8_t _msg) {
__HAL_I2C_CLEAR_FLAG(&mI2CHandle, I2C_FLAG_AF);
HAL_StatusTypeDef ret = HAL_I2C_Master_Transmit(&mI2CHandle, SHIFT_ADDRESS(_address), &_msg, 1, 100);
return ret;
}
/**
* @brief Receive one byte over I2C
* @param[in] uint8_t address The address of the I2C slave
* @param[in] uint8_t command The command for the I2C slave
* @param[out] uint8_t* data The message for the I2C slave
* @retval HAL_StatusTypeDef The status of the HAL functions that are called within this method
*
* This method will call the HAL_I2C function to receive an 8 bit message over I2C
*/
HAL_StatusTypeDef I2CCommunication::i2cRead8(uint8_t _address, uint8_t _command, uint8_t* _data) {
uint8_t ret = 0; //HAL_OK
ret |= (uint8_t)HAL_I2C_Master_Transmit(&mI2CHandle, SHIFT_ADDRESS(_address), &_command, 1, 100);
ret |= (uint8_t)HAL_I2C_Master_Receive( &mI2CHandle, SHIFT_ADDRESS(_address), _data, 1, 100);
return static_cast<HAL_StatusTypeDef>(ret);
}
/**
* @brief Receive two bytes over I2C
* @param[in] uint8_t address The address of the I2C slave
* @param[in] uint8_t command The command for the I2C slave
* @param[out] uint16_t* data The message for the I2C slave
* @retval HAL_StatusTypeDef The status of the HAL functions that are called within this method
*
* This method will call the HAL_I2C function to receive an 16 bit message over I2C
*/
HAL_StatusTypeDef I2CCommunication::i2cRead16(uint8_t _address, uint8_t _command, uint16_t* _data) {
uint8_t ret = 0; //HAL_OK
uint8_t readVal[2] = { 0 };
ret |= (uint8_t)HAL_I2C_Master_Transmit(&mI2CHandle, SHIFT_ADDRESS(_address), &_command, 1, 100);
ret |= (uint8_t)HAL_I2C_Master_Receive( &mI2CHandle, SHIFT_ADDRESS(_address), readVal, 2, 100);
*_data = (((uint16_t)readVal[1] << 8) | ((uint16_t)readVal[0] & 0xFF));
return static_cast<HAL_StatusTypeDef>(ret);
}Error I get:
../Core/Inc/I2CCommunication.h:16:36: error: expected ')' before '_hi2c'
16 | I2CCommunication(I2C_HandleTypeDef _hi2c);
| ~ ^~~~~~
| )
../Core/Inc/I2CCommunication.h:22:2: error: 'I2C_HandleTypeDef' does not name a type; did you mean 'DMA_HandleTypeDef'?
22 | I2C_HandleTypeDef mI2CHandle;
| ^~~~~~~~~~~~~~~~~
| DMA_HandleTypeDef
../Core/Src/I2CCommunication.cpp:11:35: error: expected constructor, destructor, or type conversion before '(' token
11 | I2CCommunication::I2CCommunication(I2C_HandleTypeDef _hi2c) {
| ^
../Core/Src/I2CCommunication.cpp: In member function 'HAL_StatusTypeDef I2CCommunication::i2cWrite8(uint8_t, uint8_t)':
../Core/Src/I2CCommunication.cpp:23:24: error: 'mI2CHandle' was not declared in this scope
23 | __HAL_I2C_CLEAR_FLAG(&mI2CHandle, I2C_FLAG_AF);
| ^~~~~~~~~~
../Core/Src/I2CCommunication.cpp:23:36: error: 'I2C_FLAG_AF' was not declared in this scope
23 | __HAL_I2C_CLEAR_FLAG(&mI2CHandle, I2C_FLAG_AF);
| ^~~~~~~~~~~
../Core/Src/I2CCommunication.cpp:23:2: error: '__HAL_I2C_CLEAR_FLAG' was not declared in this scope
23 | __HAL_I2C_CLEAR_FLAG(&mI2CHandle, I2C_FLAG_AF);
| ^~~~~~~~~~~~~~~~~~~~
../Core/Src/I2CCommunication.cpp:24:26: error: 'HAL_I2C_Master_Transmit' was not declared in this scope
24 | HAL_StatusTypeDef ret = HAL_I2C_Master_Transmit(&mI2CHandle, SHIFT_ADDRESS(_address), &_msg, 1, 100);
| ^~~~~~~~~~~~~~~~~~~~~~~
../Core/Src/I2CCommunication.cpp: In member function 'HAL_StatusTypeDef I2CCommunication::i2cRead8(uint8_t, uint8_t, uint8_t*)':
../Core/Src/I2CCommunication.cpp:38:43: error: 'mI2CHandle' was not declared in this scope
38 | ret |= (uint8_t)HAL_I2C_Master_Transmit(&mI2CHandle, SHIFT_ADDRESS(_address), &_command, 1, 100);
| ^~~~~~~~~~
../Core/Src/I2CCommunication.cpp:38:18: error: 'HAL_I2C_Master_Transmit' was not declared in this scope
38 | ret |= (uint8_t)HAL_I2C_Master_Transmit(&mI2CHandle, SHIFT_ADDRESS(_address), &_command, 1, 100);
| ^~~~~~~~~~~~~~~~~~~~~~~
../Core/Src/I2CCommunication.cpp:39:18: error: 'HAL_I2C_Master_Receive' was not declared in this scope
39 | ret |= (uint8_t)HAL_I2C_Master_Receive( &mI2CHandle, SHIFT_ADDRESS(_address), _data, 1, 100);
| ^~~~~~~~~~~~~~~~~~~~~~
../Core/Src/I2CCommunication.cpp: In member function 'HAL_StatusTypeDef I2CCommunication::i2cRead16(uint8_t, uint8_t, uint16_t*)':
../Core/Src/I2CCommunication.cpp:54:43: error: 'mI2CHandle' was not declared in this scope
54 | ret |= (uint8_t)HAL_I2C_Master_Transmit(&mI2CHandle, SHIFT_ADDRESS(_address), &_command, 1, 100);
| ^~~~~~~~~~
../Core/Src/I2CCommunication.cpp:54:18: error: 'HAL_I2C_Master_Transmit' was not declared in this scope
54 | ret |= (uint8_t)HAL_I2C_Master_Transmit(&mI2CHandle, SHIFT_ADDRESS(_address), &_command, 1, 100);
| ^~~~~~~~~~~~~~~~~~~~~~~
../Core/Src/I2CCommunication.cpp:55:18: error: 'HAL_I2C_Master_Receive' was not declared in this scope
55 | ret |= (uint8_t)HAL_I2C_Master_Receive( &mI2CHandle, SHIFT_ADDRESS(_address), readVal, 2, 100);
| ^~~~~~~~~~~~~~~~~~~~~~
make: *** [Core/Src/subdir.mk:41: Core/Src/I2CCommunication.o] Error 1
make: *** Waiting for unfinished jobs....
"make -j8 all" terminated with exit code 2. Build might be incomplete.I would like to ask your feedback.
I have tried fix the code but wasn't successful. That's why i would appreciate another pair of eye.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.