STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N657 IO 3.3V tolerant?

Hello,I'm using the STM32N657 processor and have the HEXASPI device running at 1.8V.  VDDIO2 is connected to 1V8 supply (which affects: PO[5..0] and PP[15..0]The FMC is placing the A23 line on pin PO1 (this is the only option for the FMC-A23) and the...

mattcrc_0-1761602911315.png
matt-crc by Senior III
  • 727 Views
  • 5 replies
  • 1 kudos

Resolved! L073: ADC & DMA, strange buffer "shift" in CIRCULAR mode

Heyho,strange things happening that I'd like to understand for a STM32L073 (Nucleo for now).Setup on a L073 @ 32MHz:- ADC is clocked by PCLK/4- ADC prescaler = 2 -> divide by 4 -> 2 MHz- 12 bit right aligned- ref V = VDDA = 3.3V- hardware oversamplin...

LCE by Principal II
  • 1672 Views
  • 15 replies
  • 2 kudos

Resolved! STM32H750 XiP Clock change

Hey together, I have a question regarding changing the clock while running in XiP mode. Upfront everything works so far very well. On our STM32H750 we have a very simple bootloader. This bootloader configures the QSPI and the STM32H7 to run the appli...

ESawa1_0-1761134946554.png
ESawa.1 by Senior
  • 1298 Views
  • 6 replies
  • 0 kudos

Resolved! Cannot enter DFU mode on STM32F446ZET6

Hi everyone, I’m working with a custom made STM32F446ZET6 board that otherwise functions perfectly (all peripherals, flash programming, etc. work fine). The only thing that doesn’t is the ROM bootloader. I can’t get USB DFU or UART boot to respond no...

samprince by Associate II
  • 2067 Views
  • 9 replies
  • 3 kudos

UART idle transmission

Hi,I'm exploring using UART idle interrupt on RX to signal to my application that data has arrived.I currently push data into a tx queue then start transmission. I rely on uart tx ISRs to check if there is any more data to send, then load up a DMA tr...

law__ by Associate II
  • 1479 Views
  • 10 replies
  • 8 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.