2025-09-22 7:55 AM
Hi,
I would like to recreate the DCMIPP_ContinuousMode example but using the cubeMX to configure the MCU, I haven't found anything online to follow as example.
Thanks.
Solved! Go to Solution.
2025-09-23 2:43 AM
Hi @BrAjN
This application note should be helpful: Introduction to digital camera interface pixel pipeline for STM32 MCUs
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-23 2:43 AM
Hi @BrAjN
This application note should be helpful: Introduction to digital camera interface pixel pipeline for STM32 MCUs
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-15 12:25 AM
Hello, about this, I have run the example code that is provided.
however I find found that the example when run on my side with out edits, produces Blurry image quality on the LCD screen.
Is this the case, or is some thing wrong with my camera module,
I have just begun development on the board.
Same thing with the snapshot decimation example.
2025-10-27 11:40 PM
Hey there @BrAjN ,
I was wondering were you have reached with this initiative.
I have also tried to recreate that same project specifically the dcmipp peripheral, but in vain.
My code runs as expected, however I think I dont have images coming through the pipe 1 on virtual channel 0,
AM using the stm32n6570 DK and the IMX335 camera module
DId you find any such case.
Attached are the files that I think will be of importance
The set frequency of the peripheral is 300MHz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.