STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4R9I_EVAL and TouchGFX EEPROM issue

I'm using the STM32L4R9I_Eval board with the STM32 Cube IDE (v 1.12.1) and the TouchGFX interface (v 4.21.3).  I'm having an issue with EEPROM... I grabbed the STM32 provided BSP EEPROM code and am basically reading/writing a structure that contains ...

Port SBSFU from STM32F413ZH example to run on NUCLEO-F429ZI

Hello everyoneI'm currently testing SBSFU, however, I'm new to ST porting stuff. I had successfully built SBSFU example for STM32F413H-Discovery with STMCubeIDE as the closest model to my target MPU which is STM32-F429ZI.I wish someone could guide me...

AliT by Associate II
  • 1371 Views
  • 1 replies
  • 0 kudos

I2S MASTER desynchronization at start

Hello,i working in I2S since 6 month on STM32F405. after several analyzes, we have problems.we work on I2S is connected on SGT5000.SGTL5000 must have continous master clock to communicate with him on I2C.So the design started I2S MASTER with DMA all ...

trave.1 by Associate II
  • 4612 Views
  • 2 replies
  • 0 kudos

Resolved! STM32, Stack-Utilization

Hello,for determining the Stack-Utilization I fill it with 0xDADBEEF. If you have recommendations and other ideas, I’d like to know and looking forward to learn from others, how they approach the issues “Stacksize” and “Stackutilization”.Code for the...

STM32CubeIDE_Deadbeef_Stack.png

JTAG Connection Lost After Successfull Programming

Dear All,My board has an STM32l072RZ mcu. I am trying to study low power modes. I created a sleep mode example and I flashed it properly. Everything looks great until this point. But, when i tried to connect after first flashing, my jtag(jlink) says ...

sorterus by Associate II
  • 2706 Views
  • 4 replies
  • 0 kudos

3-wire SPI Receive - RXNE not working

STM32G031 SPI in 3-wire half duplex mode. When reading data (BIDIMODE=1, BIDIOE=0), how can I tell when I have clocked in a complete u8/u16?Neither RXNE or FRLVL appear to get updated until I stop the transaction.I have it working by using a delay in...

STM32F767 SPI SLAVE DUMMY CYCLES AND FREQUENCY RELATION

Hi,I am using a STM32F767zi nucleo board as  SPI full duplex slave. The dummy cycles of the slave device is varies in accordance with the master frequency change. How can I handle the dummy cycles independent of master frequency? What is the solution...

X-CUBE-AUDIO spiritMP3 license

I am planning to sell an application that runs on the STM32F7 for a fee. If I use spritMP3, it will come with a license cost?X-CUBE-AUDIO spiritMP3 licenseYou mentioned here that spritMP3 is available free of charge, but I would like to confirm if th...

tuck by Associate
  • 957 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.