STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L052T6Yx usb(virtual port com) to pc

I want use this mcu STM32L052T6Yx  to communicate via usb (virtual port com ) whit pc (whith linux system operativ).THE power supply of mcu is 3.3v, can I problems if i directly connect PA11 PA12 PIN  to the pc usb (common ground)? , moreover  on pin...

Combined UAC + HID functionality with STM32L452RE

Hello,I am new to the forums here! Can STM32L452RE support a combination class of HID and USB Audio Class over USB 2.0 Fullspeed?Ideally, I'd like to read and send microphone data (or any sensor data for that matter) connected to STM32L452RE over USB...

bntess by Associate
  • 1828 Views
  • 1 replies
  • 0 kudos

SPI data size reducuction to 1-bit

I have a rather strange request, but I am communicating to a Digital Potentiometer (AD5227) over SPI.  The chip has 64 available positions, but can only increment or decremement its position by 1 for each clock cycle.  To increment by 1, a 1 is place...

JSext.1 by Associate II
  • 5734 Views
  • 12 replies
  • 1 kudos

STM32F 407 &&& 2 USB MASS STORAGE DEVICE

Good evening guys, I have an educational project for the USB protocol on the stm23f407 discovery board I made the project on two sensors and each sensor is written to a flash drive on a separate usb_otg_host port because the stm32f407 discovery board...

Resolved! STM32H723 ADC read stuck (using LL libraries)

Hello,In my project I just sometimes need to read ADC values. I figure I could simply connect two of my signals to ADC1 and ADC2 respectively.What it strange that it does sometimes working, but sometimes it is stuck at constant value ( maybe first re...

Linas L by Senior II
  • 3003 Views
  • 4 replies
  • 1 kudos

Resolved! SPI value doesn't update in STM32F746

Hello, I'm using a STEVAL-PLC001V1 card. It is based on a STM32F746ZGT7 that is linked to a CLT01-38SQ7 for inputs and ISO8200AQ for outputs, using SPI.I try to read datas sent through SPI by the CLT01-38SQ7 and then send it back to the ISO8200AQ.My ...

CGAUC.1 by Associate II
  • 3358 Views
  • 6 replies
  • 0 kudos

i am trying to wakeup stm32lo from sleep mode by interrupt push button connected to pA3

 HAL_SuspendTick();        /* Enter Sleep Mode,        *        */   HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);        /* Resume Tick interrupt if disabled prior to SLEEP mode entry */       HAL_ResumeTick();I HAVE THE ABOVE CO...

NASOK.1 by Associate II
  • 1489 Views
  • 1 replies
  • 0 kudos

Help me understand why my UART communication fails

Good morning, my product is made of 2 parts, each of which has a dedicated MCU. MCU1 is STM32L476ZG and MCU2 is STM32L4P5CG. The whole device is supplied through a wall adapter working at 24VDC. Internally,the voltage is converted to supply all the m...

mdiro by Associate III
  • 9256 Views
  • 7 replies
  • 0 kudos

CAN communication on STM32F429ZIT6 problem

Hello, I initialized CAN on STM32F429ZIT6 on registers. I would like to tranmitt and receive messages. But on transmission lines is silence. In my opinion I forgot about any register, but I don't know which. So could you help me what i sholud change ...

inic.PNG inic2.PNG inic3.PNG inic4.PNG
michal3 by Associate
  • 975 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.